2024-08-01 10:36 PM - last edited on 2024-08-02 1:54 AM by Peter BENSCH
Hello to STM community,
I am sharing my problem with you regarding STEVAL-IHP005V1 evaluation kit.
My setup:
I am using STEVAL-IHP005V1 power line communication evaluation kit.
There is a windows based GUI software provided from ST's side to communicate with this kit via RS-232 protocol.
For powering this device there are two option 12V and 3.3V.
I am powering up this device by providing 3.3V from USB-TTL module.
Till now GUI and kit are successfully communicating with each other.
I am able to set/get various parameters to a kit.
Both kit's are connected to 220V to 240V AC with 50Hz frequency power lines, via their Neutral and Live terminals.
Actual problem:
My problem here is that i want to send data from one module to another module through power lines.
I have connected kit's Live and Neutral terminals to power lines.
Broadcasting data using GUI and expecting another module to receive it and printed in GUI.
I have kept open two windows and both are separately connected to these two kits through RS-232.
The thing is till now data transmission from one node to another did not go successful not even once.
I do not have any idea how to proceed this experiment further.
Seeking help from community and ST's team.