cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F746 cannot read level of audio input signal

aciuf
Associate II

I would like to read the level of audio input signal to use like a vu-meter instead of use analog input.

 

This is my code but I read always 0dB on both channels.

 

 

void AUDIO_PLAYER_Init2()
{

/* Allocat mem for Smr */

pSmrPersistentMem = malloc(smr_persistent_mem_size); /* smr_persistent_mem_size 0x188 */

pSmrScratchMem = malloc(smr_scratch_mem_size); /* smr_scratch_mem_size 0xF04 */

 

 

if (BSP_AUDIO_IN_Init(INPUT_DEVICE_INPUT_LINE_1, 80, AUDIO_FREQUENCY_48K) != 0)

LCD_LOG_SetHeader((uint8_t *)"Audio SMR Application KO");

else

LCD_LOG_SetHeader((uint8_t *)"Audio SMR Application OK");

}

 

void Audio_Process2()
{

    int32_t error = SMR_ERROR_NONE;

    __HAL_RCC_CRC_CLK_ENABLE();

    CRC->CR = CRC_CR_RESET;

   

    error = smr_reset(pSmrPersistentMem, pSmrScratchMem);

    if (error != SMR_ERROR_NONE)

    {

        BSP_LCD_DisplayStringAt(10, 20, (uint8_t *)"--err0--", LEFT_MODE);

        return (AUDIO_ERROR_SMR);

    }

 

    smr_static_param.sampling_rate = 48000; /* only sampling rate supported */

    error = smr_setParam(&smr_static_param, pSmrPersistentMem);

    if (error != SMR_ERROR_NONE)

    {

       BSP_LCD_DisplayStringAt(10, 20, (uint8_t *)"--err1--", LEFT_MODE);

       return (AUDIO_ERROR_SMR);

    }

    smr_dynamic_param.enable = 1; /* SMR module enabler */

    smr_dynamic_param.averaging_time = AUDIO_CFG_SMR_AVGTIME_DEFAULT;

    smr_dynamic_param.filter_type = SMR_PREFILTER_AWEIGHTING;

 

    error = smr_setConfig(&smr_dynamic_param, pSmrPersistentMem);

    if (error != SMR_ERROR_NONE)

    {

        BSP_LCD_DisplayStringAt(10, 20, (uint8_t *)"--err2--", LEFT_MODE);

       return (AUDIO_ERROR_SMR);

    }

    error = smr_getConfig(&smr_dynamic_param, pSmrPersistentMem);

    if (error != SMR_ERROR_NONE)

    {

       BSP_LCD_DisplayStringAt(10, 20, (uint8_t *)"--err4--", LEFT_MODE);

       return AUDIO_ERROR_SMR;

   }

 

   BufferHandler.nb_bytes_per_Sample = 2; /* 16-bit */

   BufferHandler.nb_channels = 2; /* stereo */

   BufferHandler.data_ptr = PCM_Data_SMR;

   BufferHandler.buffer_size = 32/2; /* just half buffer is process (size per channel) */

   BufferHandler.mode = INTERLEAVED;

   BufferHandler.data_ptr = &BufferCtl.buff[AUDIO_OUT_BUFFER_SIZE /2];

 

   error = smr_process(pBufferHandler, pBufferHandler, pSmrPersistentMem);

   if (error != SMR_ERROR_NONE)

  {

     BSP_LCD_DisplayStringAt(10, 20, (uint8_t *)"--err5--", LEFT_MODE);

     return (AUDIO_ERROR_SMR);

  }

 

   error = smr_getConfig(&smr_dynamic_param, pSmrPersistentMem);

   if (error != SMR_ERROR_NONE)

   {

      BSP_LCD_DisplayStringAt(10, 20, (uint8_t *)"--err6--", LEFT_MODE);

      return AUDIO_ERROR_SMR;

   }

 

sprintf((char *)str_pwr, "Left mean power: %ld dB",(int32_t)((float)smr_dynamic_param.mean_level_left*0.25));

BSP_LCD_DisplayStringAt(CHAR(0), LINE(10), (uint8_t *)str_pwr, LEFT_MODE);

sprintf((char *)str_pwr, "Right mean power: %ld dB",(int32_t)((float)smr_dynamic_param.mean_level_right*0.25));

BSP_LCD_DisplayStringAt(CHAR(0), LINE(11), (uint8_t *)str_pwr, LEFT_MODE);

}

14 REPLIES 14
KnarfB
Super User

BSP_AUDIO_IN_Init(INPUT_DEVICE_INPUT_LINE_1, 80, AUDIO_FREQUENCY_48K)

doesn't match the implentation in 

32f746gdiscovery-bsp/stm32746g_discovery_audio.c at 64c20f758a907cd873e368502cf16e498934d0ec · STMicroelectronics/32f746gdiscovery-bsp (github.com)

hth

KnarfB

Andrew Neil
Super User

@aciuf wrote:

I would like to read the level of audio input signal


What "audio input signal"? On what board?

https://community.st.com/t5/community-guidelines/how-to-write-your-question-to-maximize-your-chances-to-find-a/ta-p/575228

 


@aciuf wrote:

but I read always 0dB on both channels.


Have you checked that there is actually any signal present at all?

Is the signal sufficient to read above 0 dB ?

 


@aciuf wrote:

This is my code 


So what testing / investigation / debugging have you done on your code to find what's wrong with it?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

I am using a STM32F746-DISCO so INPUT_DEVICE_INPUT_LINE_1 should be the line input.

Now I see some values but still not good

 

 

 

void  AUDIO_PLAYER_Init2()
{
	int32_t error = SMR_ERROR_NONE;

	pSmrPersistentMem = malloc(smr_persistent_mem_size); /* smr_persistent_mem_size  0x188 */
	pSmrScratchMem = malloc(smr_scratch_mem_size);       /* smr_scratch_mem_size  0xF04 */


	if (BSP_AUDIO_IN_Init(INPUT_DEVICE_INPUT_LINE_1, 100, AUDIO_FREQUENCY_48K) != 0)
	//if (BSP_AUDIO_IN_Init(INPUT_DEVICE_DIGITAL_MICROPHONE_2, 80, AUDIO_FREQUENCY_48K) != 0)
		LCD_LOG_SetHeader((uint8_t *)"Audio SMR Application KO");
	else
		LCD_LOG_SetHeader((uint8_t *)"Audio SMR Application OK");

	 __HAL_RCC_CRC_CLK_ENABLE();

	CRC->CR = CRC_CR_RESET;

	error = smr_reset(pSmrPersistentMem, pSmrScratchMem);
	if (error != SMR_ERROR_NONE)
	{
	 	BSP_LCD_DisplayStringAt(10, 20, (uint8_t *)"--smr_reset--", LEFT_MODE);
	    return (AUDIO_ERROR_SMR);
	}

	smr_static_param.sampling_rate = 48000;   /* only sampling rate supported */

	error = smr_setParam(&smr_static_param, pSmrPersistentMem);
	if (error != SMR_ERROR_NONE)
	{
	   BSP_LCD_DisplayStringAt(10, 20, (uint8_t *)"--smr_setParam--", LEFT_MODE);
	   return (AUDIO_ERROR_SMR);
	}

	/* SMR dynamic parameters that can be updated here every frame if required */
	smr_dynamic_param.enable = 1;                        /* SMR module enabler */
	smr_dynamic_param.averaging_time = AUDIO_CFG_SMR_AVGTIME_DEFAULT;
	smr_dynamic_param.filter_type = SMR_PREFILTER_AWEIGHTING;

	error = smr_setConfig(&smr_dynamic_param, pSmrPersistentMem);
	if (error != SMR_ERROR_NONE)
	{
		BSP_LCD_DisplayStringAt(10, 20, (uint8_t *)"--smr_setConfig--", LEFT_MODE);
	    return (AUDIO_ERROR_SMR);
	}
	/* I/O buffers settings */
	BufferHandler.nb_bytes_per_Sample = 2;			/* 16-bit */
	BufferHandler.nb_channels = 2; 					/* stereo */
	BufferHandler.data_ptr = PCM_Data_SMR;
	BufferHandler.buffer_size = 32/2; 		/* just half buffer is process (size per channel) */
	BufferHandler.mode = INTERLEAVED;
}

void Audio_Process2()
{
	int32_t error = SMR_ERROR_NONE;

	uint16_t pbuf[100];

    error = smr_process(pBufferHandler, pBufferHandler, pSmrPersistentMem);
	if (error != SMR_ERROR_NONE)
    {
	    BSP_LCD_DisplayStringAt(10, 20, (uint8_t *)"--smr_process--", LEFT_MODE);
        return (AUDIO_ERROR_SMR);
    }

    error = smr_getConfig(&smr_dynamic_param, pSmrPersistentMem);
    if (error != SMR_ERROR_NONE)
    {
    	BSP_LCD_DisplayStringAt(10, 20, (uint8_t *)"--smr_getConfig--", LEFT_MODE);
        return AUDIO_ERROR_SMR;
    }
    sprintf((char *)str_pwr, "Left mean power:  %ld dB",(int32_t)((float)smr_dynamic_param.mean_level_left*0.25));
    BSP_LCD_DisplayStringAt(CHAR(0), LINE(10), (uint8_t *)str_pwr, LEFT_MODE);
    sprintf((char *)str_pwr, "Right mean power:  %ld dB",(int32_t)((float)smr_dynamic_param.mean_level_right*0.25));
    BSP_LCD_DisplayStringAt(CHAR(0), LINE(11), (uint8_t *)str_pwr, LEFT_MODE);
}

@aciuf wrote:

Now I see some values


So what did you change?

 


@aciuf wrote:

 but still not good


In what way, "not good"?  Give numbers!

Again, are you sure that the input signal you're providing is adequate?

 


@aciuf wrote:

so INPUT_DEVICE_INPUT_LINE_1 should be the line input.


and are you actually feeding it a good, line-level signal?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
aciuf
Associate II

Using this last code the dB print without input signal start from 0dB and decrease

https://youtu.be/PohM2AMRxFI

aciuf
Associate II

In the main I call at the begin

AUDIO_PLAYER_Init2

and in a loop

Audio_Process2

 

 

 

So what did you change?

I have insert only 2 fuctions in the loop

aciuf
Associate II

New version

Now I see some correlation from input signal and dB print but still not correct

 

void *pSmrPersistentMem = NULL;
void *pSmrScratchMem = NULL;

static  smr_static_param_t smr_static_param;
static  smr_dynamic_param_t smr_dynamic_param;

static  buffer_t BufferHandler;
static  buffer_t *pBufferHandler = &BufferHandler;

static  uint8_t str_pwr[100];

uint16_t PCM_Data_SMR[32]; 		/* PCM data buffer */



void  AUDIO_PLAYER_Init2()
{
	int32_t error = SMR_ERROR_NONE;

	pSmrPersistentMem = malloc(smr_persistent_mem_size); /* smr_persistent_mem_size  0x188 */
	pSmrScratchMem = malloc(smr_scratch_mem_size);       /* smr_scratch_mem_size  0xF04 */


	if (BSP_AUDIO_IN_Init(INPUT_DEVICE_INPUT_LINE_1, 100, AUDIO_FREQUENCY_48K) != 0)
	//if (BSP_AUDIO_IN_Init(INPUT_DEVICE_DIGITAL_MICROPHONE_2, 80, AUDIO_FREQUENCY_48K) != 0)
		LCD_LOG_SetHeader((uint8_t *)"Audio SMR Application KO");
	else
		LCD_LOG_SetHeader((uint8_t *)"Audio SMR Application OK");

	 __HAL_RCC_CRC_CLK_ENABLE();

	CRC->CR = CRC_CR_RESET;

	error = smr_reset(pSmrPersistentMem, pSmrScratchMem);
	if (error != SMR_ERROR_NONE)
	{
	 	BSP_LCD_DisplayStringAt(10, 20, (uint8_t *)"--smr_reset--", LEFT_MODE);
	    return (AUDIO_ERROR_SMR);
	}

	smr_static_param.sampling_rate = AUDIO_FREQUENCY_48K;   /* only sampling rate supported */

	error = smr_setParam(&smr_static_param, pSmrPersistentMem);
	if (error != SMR_ERROR_NONE)
	{
	   BSP_LCD_DisplayStringAt(10, 20, (uint8_t *)"--smr_setParam--", LEFT_MODE);
	   return (AUDIO_ERROR_SMR);
	}

	/* SMR dynamic parameters that can be updated here every frame if required */
	smr_dynamic_param.enable = 1;                        /* SMR module enabler */
	smr_dynamic_param.averaging_time = 100; //AUDIO_CFG_SMR_AVGTIME_DEFAULT;
	smr_dynamic_param.filter_type = SMR_PREFILTER_AWEIGHTING;

	error = smr_setConfig(&smr_dynamic_param, pSmrPersistentMem);
	if (error != SMR_ERROR_NONE)
	{
		BSP_LCD_DisplayStringAt(10, 20, (uint8_t *)"--smr_setConfig--", LEFT_MODE);
	    return (AUDIO_ERROR_SMR);
	}
	/* I/O buffers settings */
	BufferHandler.nb_bytes_per_Sample = 2;			/* 16-bit */
	BufferHandler.nb_channels = 2; 					/* stereo */
	//BufferHandler.data_ptr = PCM_Data_SMR;
	BufferHandler.buffer_size = 32/2; 		/* just half buffer is process (size per channel) */
	BufferHandler.mode = INTERLEAVED;
}

void Audio_Process2()
{
	int32_t error = SMR_ERROR_NONE;

	BSP_AUDIO_IN_Record(&BufferCtl.buff[0], 32/2);

	BufferHandler.data_ptr = &BufferCtl.buff[0];

    error = smr_process(pBufferHandler, pBufferHandler, pSmrPersistentMem);
	if (error != SMR_ERROR_NONE)
    {
	    BSP_LCD_DisplayStringAt(10, 20, (uint8_t *)"--smr_process--", LEFT_MODE);
        return (AUDIO_ERROR_SMR);
    }

    error = smr_getConfig(&smr_dynamic_param, pSmrPersistentMem);
    if (error != SMR_ERROR_NONE)
    {
    	BSP_LCD_DisplayStringAt(10, 20, (uint8_t *)"--smr_getConfig--", LEFT_MODE);
        return AUDIO_ERROR_SMR;
    }
    sprintf((char *)str_pwr, "Left mean power:  %ld dB",(int32_t)((float)smr_dynamic_param.mean_level_left*0.25));
    BSP_LCD_DisplayStringAt(10, 100, (uint8_t *)str_pwr, LEFT_MODE);
    sprintf((char *)str_pwr, "Right mean power:  %ld dB",(int32_t)((float)smr_dynamic_param.mean_level_right*0.25));
    BSP_LCD_DisplayStringAt(10, 120, (uint8_t *)str_pwr, LEFT_MODE);
}