Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

OPC on II3SDWB

Dear Sirs,I would ask haw to perform OPC (one point calibration) in II3SDWB sensor.In datasheet and also in AN5444 is mentioned but not described.Thanks. 

mruppi by Associate
  • 578 Views
  • 0 replies
  • 0 kudos

SPI EEPROM M95512-W

Hello, I am trying to write to this EEPROM and when I do, what I read back is always some other data, as if the EEPROM is write protected. The sequence of instructions I am using are:   CMD 0x06 - Write Enabke CMD 0x05 - Read status register, returns...

Есть ли возможность связаться с отделом разработки?

Непосредственный вопрос, как можно связаться с отделом, который занимается разработкой разного рода отладочных плат и демонстрационных образцов?у меня есть предложение. как я понял. представители st здесь присутствуют, и возможно помогут выйти на диа...

mpp2508 by Associate
  • 738 Views
  • 1 replies
  • 0 kudos

Resolved! M9510-W data is not written correctly

I have a design that used an M95010-W and can read the Status as well as set the WEL bit and read it back in the status.  However when I try to write data starting at address 0 with the command string 0x02 0x00 followed by data in the same SPI frame ...

Resolved! How to load a firmware from M95P32 EEPROM ?

Hello,I need to and a FOTA to my application.I will receive the firmware with BLE and store it on M95P32 EEPROM. Then i need to load it on the mcu (STM32WL).I cannot find any example or resources that explain how can i  load a firmware from M95P32 EE...

malarab by Senior II
  • 1167 Views
  • 1 replies
  • 0 kudos