Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STUW81300 STWPLLSim

 Hello.I want to use STUW81300 to create 9 GHz with great phase noise.Reference: 50 MHzPDF:50MHzSingle-EndedSTWPLSim v5.3 was used for the loop filter design.However, the actual measurements were 3~7dB worse than the simulated values.All settings see...

hccho by Associate
  • 749 Views
  • 1 replies
  • 0 kudos

Specs for EXTVCO_IN for STW81200

Both STuW81300 and STW81200 have the option of using an external VCO but the inputs characteristics aren't specified anywhere. What is the input frequency range, input power/sensitivity in dBm or 50ohm match for single-ended input? There is one appli...

mallets by Associate
  • 483 Views
  • 1 replies
  • 0 kudos

Resolved! Replacement for BMO055

Dear forumI need to update a board that uses BMO055 9 axis IMU and I need to know what is the preferred ST solution that best fit this obsoleted part.I need the 3 axis gyro + 3axis accelerometer + 3 axis magnetometerIf there is a single chip solution...

nachus001 by Associate II
  • 1151 Views
  • 6 replies
  • 0 kudos

M41ST87W RTC Module Read problem

We use M41ST87W as RTC module. We set the stop bit (ST) to 0. We can also observe the frequency at the F32K output. We constantly read the Second register but we do not see any change. What could be the reason for this?

elehab by Associate
  • 368 Views
  • 2 replies
  • 0 kudos

Resolved! COREMP135 software

I purchase one M5STAck COREMP135, it noticed work for linux, but when I use the software, it can't handle user account , only use root login.Then I try build image by myself, the github support was 2-3 years ago.I see one training company - Bootlin s...