Automotive MCUs

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! SPC58xHx BAF code loops in infinitely after reset or re-powered

Dear Experts,After erasing all flash, I flash new program to SPC58 and it can just work as soon as flashing the application execution file (e.g. elf).My SPC58 cannot run the application code after reset or re-powered.Based on the SPC58 H Line Referen...

0693W00000HrBs3QAF.png
HNguy.20 by Associate
  • 953 Views
  • 2 replies
  • 0 kudos

Resolved! MCAL drivers for SPC560 and SPC563

We have MCAL drivers for MPC560 and MPC563 microcontrollers (AUTOSAR 3.0 and 4.0).Can we use them to write MCAL drivers for SPC560 and SPC563 microcontrollers?

Resolved! SPC5 MCAL Driver

I want SPC56, SPC57 and SPC58 MCAL for AUTOSAR 3.0 and 4.0 (STSW-SPC5-MCAL)(Of course the microcontroller that I use, is SPC563M64L5)Please advise me how to prepare it.

Resolved! MCAL Driver

I want SPC56, SPC57 and SPC58 MCAL for AUTOSAR 3.0 and 4.0 (STSW-SPC5-MCAL)(Of course the microcontroller that I use, is SPC563M64L5)Please advise me how to prepare it.

Resolved! SPC560P50L5 & MPC560

I am using SPC560P50L5 microcontroller.Can I code with MPC560 microcontrollers and CodeWarriorIDE software and transfer the hex file to SPC560P50L5 microcontroller???

Resolved! SPC56XX JTAG Password Send Sequence

I have a SPC56XX part which I need to unlock for a JTAG OnCE debug session.The procedure for enabling debug on a locked device is described in AN4035, however when I follow the steps I get no response from the MCU when sending correct password. Is th...

tbnkr by Associate II
  • 1296 Views
  • 2 replies
  • 0 kudos

Resolved! SPC5 Motor Control Live Monitor location?

​Hello ST Community,​Documentation for the Motor Control Toolkit and L9907 often reference a SPC5 Motor Control Live Monitor. Is the Live Monitor still downloadable from somewhere, even if we have not bought the kit with a motor, L9907 and SPC560P? T...

EPelt.1 by Associate II
  • 1626 Views
  • 8 replies
  • 0 kudos