Automotive MCUs

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! Hello, I use the L9963e-mcu evaluation board to test behavior of the stack monitor wich is embedded on it. I want to recover the sources of the executable embedded in the SPC574S64E3, I only have the ELF, "BMS_L9963T_ver_1.6.elf".

I use the L9963E GUI PC tools to configure/communicate with the ST µc SPC574S64E3, it works fine. I know want to learn more about the communication between the µC and the stack monitor component.Thanks in advance

Resolved! Monitor registers of MCU in UDE STK

Hello.Is there in way to watch or monitor the registers or receive/transmit buffers in UDE STK when MCU is working? There was a watch or Peripheral Registers windows but nothing similar data received.Would you please help me out with this.​Thanks.​

DNewm.1 by Associate III
  • 521 Views
  • 1 replies
  • 0 kudos

Resolved! SPC58NN cannot debug after flash DCF

Debug tool:Lauterbach  Software Version: R.2018.02.000096069The screenshot of CMM is as follows:Of course, this cmm is modified by the cmm of the MPC5xxx chipThe above script writes two addresses,0x00400360, the write data is 0x05AA55AF000000000x0040...

0693W00000NrSGtQAN.jpg 0693W00000NrSGyQAN.jpg 0693W00000NrSJYQA3.png 0693W00000NrSJiQAN.png
XJian.1 by Associate
  • 567 Views
  • 1 replies
  • 0 kudos

Resolved! Hi, I'm evaluating a solution for a 1 ms reading using the SDADC driver provided with the SPC Studio (SPC58NE). I found this check in the code, that sometimes causes a missing reading. I add a comment with the SFR register that I'm currently using.

uint8_t sdadc_lld_read(SDADCDriver *sdadcp, float* converted_value) {   int16_t data; uint8_t return_value = SDADC_DATA_NOTVALID;   /* check if valid data is available */ if (sdadcp->sdadc->SFR.B.DFEF == 0U) /* <- Check if the FIFO is not emp...

VBOSC.1 by Associate
  • 928 Views
  • 2 replies
  • 0 kudos

Resolved! UDE starterkit debugging problem

I am using SPC58EC disp board. I can upload code and see led is linking when I reset the board. But I can not debug it, my code’s start location is 0x01020000 but it is going somewhere else. I asked if I can set debug start location to PLS and they s...

kb24 by Senior
  • 764 Views
  • 2 replies
  • 0 kudos

Resolved! Alternate for ST10R

Hi Team,We are using ST10R167 in our design, as you that it is obsolete right now. So we have chosen an Alternate MCU, Part Number:SPC560P50L5CEFAR.Please let me know the Year to End of Life of the selected MCU and your comments on this Alternate.Loo...

GPand.3 by Associate II
  • 611 Views
  • 1 replies
  • 0 kudos

How can i use flexray on SPC584B-DISP development board?

Hello , i bought one SPC584B-DISP discovery board. And i think there is a Flexray Peripheral mcu on the board because mentioned that on ST's website: SPC584B-DISP - SPC584B-DISP: Discovery kit featuring SPC58 4B Line MCU in eTQFP144 - STMicroelectron...

AYazı.3 by Associate II
  • 605 Views
  • 1 replies
  • 0 kudos
coolboy by Associate
  • 827 Views
  • 2 replies
  • 0 kudos