Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

SPC5-UDESDK JTAG debugger stopped working after PC was rebooted.

I am setting up a development environment with SPC5-Studio, Discovery Plus Kit for SPC56 L line (with SPC56EL70L5 MCU) and SPC5-UDESDK JTAG debugger.Initially I was able to set up the SPC5-Studio and upload an example application (LED blinker), but a...

KShar.5 by Associate II
  • 2331 Views
  • 7 replies
  • 1 kudos

Spi receive data fault

Hello ​I'm using spc560p40 and I tried to read data from other slave. When I monitor the code on logic analyzer, data is OK, but my mcu saw data one shift to right. I used spi_dll_exchange(&SPID, 2 , TX BUFFER, RX BUFFER) to send and receive data. Wo...

DNewm.1 by Associate III
  • 669 Views
  • 0 replies
  • 0 kudos

uC Hard reset occurs when put uC into Standby mode

Hello, i am Tuan from FPT.We are currently using SPC58EC for our project and the issue is HARD RESET occurs after we send request to put uC into Standby mode.It may work sometimes but usually reset uC. So do we have to check for any condition to make...

TNguy.47 by Associate
  • 514 Views
  • 0 replies
  • 0 kudos

Resolved! Application configuration

when i configure spc58nn project ,there is pineditor and clock tree ,the configurtion gui. and i cant find any other peripheral configuration gui,any one know this?

szhan.7 by Associate II
  • 2570 Views
  • 11 replies
  • 0 kudos