Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

SP582B MCAL error

Hello,When we are using SPC582B MCAL, we see that the manual only supports 32 Transmit Buffers for one way CAN, but we need to use 38 Transmit Buffers on BCAN. When I import ARXML into EB and generate CAN configuration parameters, EB will report an e...

0693W00000aInkcQAC.png 0693W00000aInkrQAC.png
ligbt.1 by Associate
  • 970 Views
  • 0 replies
  • 0 kudos

I am configuring the flexray controller.After setting the parameters, a RUN command is given which changes the POC_state from POC:ready to POC:startup. But further change of state to POC:normalactive is not observed.

The FlexRay cluster I have here consist of 2 FlexRay cold-start nodes and the third node, spc58ec mcu non-cold start node. Can anybody suggest what can go wrong ?

RSeba.2 by Associate III
  • 3411 Views
  • 4 replies
  • 0 kudos