Microcontrollers

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Regarding the issue with the SPC5-UDESTK

I am facing an issue while I am checking the local variables while debugging using the SPC5-UDESTKIt updates the variables but not the values of all of them. I have attached a snippet of the Locals Window along with this email for your reference.Can ...

0693W00000QMwtRQAT.png
RKuma.16 by Associate
  • 324 Views
  • 2 replies
  • 0 kudos

Resolved! ADC library header

Hi, i want to ask regarding the sensor library. As i new to SPC5Studio, i want to connect the displacement sensor. So , do i need to declare the sensor library as a header or just simply can use the ADC header library?

Angle by Associate II
  • 545 Views
  • 3 replies
  • 0 kudos

Resolved! irqIsrEnable Debug Crash

Hi,i have spc560p50l5 if i enable irqIsrEnable(); in debug it crash. (no codes execuded after).If i comment //irqIsrEnable(); debug works, but osal not starts.In assembly code of swirq_enable there are a lot OF_SE_ILLEGAL0x400001E8 00 00    SE_ILLEGA...

eirq interrupt

Hi, can anyone share to me the code for push button that using eirq interrupt? I do see on the example and also successfully build with no error. But when i debug and try to my hardware, nothing happened. LED do not blink when i click on push button

Angle by Associate II
  • 289 Views
  • 1 replies
  • 0 kudos

1. to make non cache area in the SPC58NH, making memory attribute to Cache-inhibit is right? 2. what is difference between data descriptors and shared descriptors? 3.The SPC58NH does not support write-through attribute for cache? if can how?

1. to make non cache area in the SPC58NH, making memory attribute to Cache-inhibit is right?2. what is difference between data descriptors and shared descriptors?3.The SPC58NH does not support write-through attribute for cache? if can how? 

Calculating faster

Hello,​ I'm working with spc560p and I want to calculate my code my code more faster as usual. I Impelement PIT DRIVER too for other use of my mcu. Is there any method to calculating faster?​Thanks for your attention

DNewm.1 by Associate III
  • 471 Views
  • 1 replies
  • 0 kudos