Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! OpenOCD works For Spc57 family?

I read from the OpenOCD docs in spc5 studio, I can only found sample instructions OpenOCD for spc58 family. But can't find any info about spc57 family support. Did spc5 studio openocd also working for other spc5 mcu family? 

jmary by Associate III
  • 1699 Views
  • 1 replies
  • 0 kudos

Resolved! SPC58 : how to measure execution time?

I use SPC58nh-disp.I use "time.h" and clock() function.but occur errorlike" c:/spc5studio-6.0/eclipse/plugins/com.st.tools.spc5.tools.gnu.gcc.ppcvle.win32_4.9.4.20200908161514/toolchain/bin/../lib/gcc/powerpc-eabivle/4.9.4/../../../../powerpc-eabivle...

hans536 by Associate III
  • 1387 Views
  • 1 replies
  • 1 kudos

Resolved! ELF File, what to do with it?

I am a bit too new to this St universe, could someone please point ,me in the right direction?I would like to update the Firmware on my BMS L9963 board. I found a folder on the website for the GUI for download. It contains a ELF file and some .dllsHo...

Orbiter by Senior
  • 2170 Views
  • 3 replies
  • 1 kudos

Resolved! Transmit SPI data from timer interrupt, the mcu become freeze

I tried to periodically send SPI data using PIT timer on SPC572.but whenever the timer interrupt call the SPI to transmit the data, the MCU freezing. while, when call the SPI transmit from main function, it working fine.any suggestion to solve this i...

jmary by Associate III
  • 2708 Views
  • 5 replies
  • 1 kudos

SPI IRQ delay

Hi all,I'm working on SPI communication between SPC582B and peripherals. I succesfully made it but I've found,  delay between characters sent by CPU is about 8us in 1MBit mode. Delay between last transmitted bit and tfff (transmit FIFO not full) is a...

Resolved! SPC5Studio FreeGcc ToolChain

Hi,i used SPC5Studio 5.8.1 for many years, but today (after windows update) in Properties->Tool Chain Editor->Current toolchain->"No ToolChain".This means that i have no possibility to change Build Settings. The same things also in SPC5Studio 6.Of co...

ck182 by Associate II
  • 3591 Views
  • 3 replies
  • 1 kudos

SPC584B Serial-Rx DMA Idle Interrupt

Hi. I am currently working on a project that involves implementing a data reception feature using the SPC584B-DISP board and the example application "RLA Serial DMA Test Application for Discovery 2."The objective is to efficiently receive approximate...

grantLim by Associate
  • 1064 Views
  • 1 replies
  • 0 kudos

Flash (NVM) of SPC564L70

Hi1) Is there specific document available for Flash (NVM) Access and Operation.2) What is the default value of NVM @ Power On?3) Error handling while programming the NVMThan you

SSJP by Associate
  • 818 Views
  • 1 replies
  • 0 kudos

DMA-SPI-SPC58 DBE error

Hi guys,In my project, i am implementing DMA-SPI Tx/Rx for SPC58NH.Interrupt SPI is verified. Communication is checked.Problem is when i activate DMA for specific SPI channel, it triggers DBE(destination Bus Error).For example, DMA ch 12(DMACHMUX_0) ...

YJ_Joe by Associate
  • 1280 Views
  • 1 replies
  • 0 kudos