cancel
Showing results for 
Search instead for 
Did you mean: 

VL53L0CXV0DH/1 issue after production

Gaston
Senior

I've manufactured 160 boards implementing the VL53L0CXV0DH/1. Many work as expected but some of them (approximately 50 units) give 8191 always as a result. I've noticed that these devices should be treated carefully using a recommended reflow profile. Also they are susceptible to shock damage.

What could be the cause of the result being 8191, in those defective devices?

Gaston_0-1698267119207.png

thanks in advance,
gaston

1 REPLY 1
Zhiyuan.Han
ST Employee

Hi Gaston

Normally 8191 means no target was detected, is it possible to log more information from RangingMeasurementData to help understand your issue? such as return signal rate, range status etc. 

 

ZhiyuanHan_0-1704939706117.png

 

Br

Zhiyuan.Han


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.