Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! X-NUCLEO-53L8A1 with NUCLEO-F401RE on Ubuntu

 Hello everyone,I am very new to the STM ecosystem and don’t know much about it. I am using an Ubuntu PC and trying to work with the X-NUCLEO-53L8A1 expansion board and NUCLEO-F401RE.There is a software package available for VL53L8CX to detect the pr...

kgb by Associate III
  • 1549 Views
  • 2 replies
  • 2 kudos

Connect SATEL board? MZ-AI EVK

I want to connect a vl53l8 satel board to the x nucleo 53L8A1, and I want to use the MZ-AI EVK software to record measurements of the external sensor, is this possible?

ay0and0 by Associate II
  • 847 Views
  • 1 replies
  • 0 kudos

Sensor to detect plastic film, edge detection

Hello,  Could someone please recommend a TOF sensor(or other) for reliable plastic sheet detection.Application: Measure the width of a sheet or film of plastic in production environment.  We would use  two sensors to detect the edges of the film.  We...

MyMack by Associate II
  • 4401 Views
  • 12 replies
  • 0 kudos

About VL53L4CX -Getting the best single-target data

Hi,I have two questions to ask.1、How do I adjust "VL53LX_MAX_RANGE_RESULTS"and "VL53LX_MAX_USER_ZONES" if I want to get a best single target of data?Would it be better to change them all to 1? It's not in the manual.2、VL53L1CB has a single-target get...

Wwei by Associate
  • 1712 Views
  • 2 replies
  • 0 kudos

Resolved! VL53L0X - measuring ball position in plexiglass tube

We are trying to assemble a laboratory plant from https://github.com/gergelytakacs/AutomationShield/wiki/FloatShieldThe ball position sensor (VL53L0X) is positioned at the top of the transparent policarbonate tube. We checked the reported ball positi...

71251627-26342300-2323-11ea-9496-1c5d9f2872e3 results_sensor.png
matevzb by Associate II
  • 936 Views
  • 1 replies
  • 0 kudos

Resolved! VL53L7CX clean room requierment

Hello,We are investigating the VL53L7CX presence detection ToF sensor. In the datasheet its mentioned it needs to be mounted in a clean environment "The customer is advised to use a clean assembly process until aprotective cover glass is mounted." an...

Resolved! Receiving VL53L7CX sensor ranging result with status 0 only

Hi all, I'm using pololu VL53L7CX sensor carrier board interfaced with Nucleo-L552zeq EVK for ranging application. For first level, iam using the Simple ranging application that comes with software package. Sensor api calls till getting the data seem...

Aju004 by Associate
  • 1793 Views
  • 4 replies
  • 0 kudos

VL53L4CX Setup Problems / Hard Fault?

Hello, I am having trouble with the VL53L4CX Sensor for my Capstone Design Project. My group created our own breakout board for the sensor, and I was able to get it up and running with the VL53L4CX_SimpleRanging project provided by ST.However, I am h...

cory9_1-1740376058750.png cory9_3-1740376144306.png cory9_4-1740376180798.png cory9_5-1740376201638.png
cory9 by Associate
  • 1485 Views
  • 3 replies
  • 0 kudos