Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Ranging results values for VL53L4CD

Hi,I am getting started with VL53L4CD so as to improve our system under ambient daylight conditions, which is performing poorly due to current sensor VL6180x under such condditions.My application is:Waking up device when target detected closer than 1...

Jhern.1 by Associate II
  • 3134 Views
  • 5 replies
  • 0 kudos

Changing the cross-talk calibration distances for the VL6180X

Hello!So in the project I am working on, we are using ToF sensors (with a cover glass) to accurately measure the distance of a white object within the ranges of 30-70mm. We would like to create a calibration fixture that also falls within these dista...

AGome.7 by Associate II
  • 1707 Views
  • 2 replies
  • 0 kudos

VL53L1X People Counting range status

Dear,What are the best practices for the people counting algorithm regarding range status? I often get status 2, so I lowered the signal threshold to 400. This reduced it, but did not solve it completely. What status codes should I allow, and which o...

SBann.1 by Associate II
  • 3560 Views
  • 7 replies
  • 0 kudos

Resolved! VL53L1X problem with write value to register

Hello, I solve a problem with writing the value to the register of sensor VL53L1X. It is the main purpose, why the sensor doesn´t read distance because the init state is invalid. For example, I tried to write the value 0x2 to the register 0x30 on the...

0693W00000Y7UChQAN.png 0693W00000Y7UFzQAN.png
toman by Associate II
  • 2438 Views
  • 4 replies
  • 0 kudos

Resolved! Finding the VL53L1X XTALK calibration distance

I am trying to perform the XTALK calibration for my system that includes a coverglass on top of the sensor. I am not exactly sure what the point of calibration should be. I've read in the forum: "When doing crosstalk calibration you need to find a ta...

0693W00000Y8QTuQAN.png 0693W00000Y8QUEQA3.png 0693W00000Y8QysQAF.png
MRoso.1 by Associate II
  • 3730 Views
  • 6 replies
  • 0 kudos

Timing budget not kept in VL53L1X

I am trying to get consecutive measurements from the VL53L1X sensor but the timing budget is only kept on the first measurement with the below codeVL53L1X_BootState(dev, &sensorState); VL53L1X_SensorInit(dev); VL53L1X_SetDistanceMode(dev, 2); VL53L1X...

0693W00000Y8L5PQAV.png
MRoso.1 by Associate II
  • 4308 Views
  • 8 replies
  • 0 kudos