2023-01-11 12:09 AM
I'm using a VL53L1X ToF sensor to measure distance with the Ultra Lite driver. I've lowered the signal threshold to 400 because that value seems to cover most valid measurements. When I read the current signal value using GetSignalRate(). When my signal rate is, for example, 600, I still get range status 2 (signalfail). What causes this?
Code I use to measure:
Sensor->Begin();
Sensor->SetTimingBudgetInMs(500);
Sensor->SetSignalThreshold(400);
Sensor->StartRanging();
Sensor->getDistanceOptimal(DistanceMM, SensorStatus);
Sensor->StopRanging();And my getDistanceOptimal() method:
this->SetDistanceMode(EDistanceMode::Short);
uint8_t dataReady = false;
while(!dataReady) {
this->CheckForDataReady(&dataReady);
//code for 5 ms delay here
}
this->GetDistanceInMm(&distance);
this->GetRangeStatus(&status);
//Retry with higher distancemode
if(status != ERangeStatus::RangeValid) {
this->SetDistanceMode(EDistanceMode::Long);
//code for 100ms delay here
this->ClearInterrupt();
while(!dataReady) {
this->CheckForDataReady(&dataReady);
//code for 5ms delay here
}
this->GetDistanceInMm(&distance);
this->GetRangeStatus(&status);
}
this->ClearInterrupt();
2023-01-11 4:47 AM
It does work when I reset my microprocessor. Any idea what causes it to be ignored until I reset?
2023-01-11 6:45 AM
Oooh boy, good old abstracted from the real world C++.
Have you tried Sensor->PleaseWork()?
Just kidding
which mcu are you using to read the sensor? Is it a custom board or a ST's nucleo/discovery?
2023-01-11 6:47 AM
Custom board with a ATSAM4LS2B. I think it's probably caused by a wrong order of method calls.
2023-01-11 8:42 AM
Okay its a microchip mcu then.
>>wrong order of method calls.
Maybe, where did you took this code from?
If you dig long enough , are you able to get to the C(baremetal) I2c configuration and operation routines?
2023-01-12 5:30 AM
Code is written by me. I can reach the i2c configuration of the ULD.
2023-01-12 5:47 AM
@John E KVAM Can you maybe help me further? I'm thinking the setsignalthreshold and getsignalrate represent different values? And does changing setsignalthreshold even help (for removing status 2) when using my code?