Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Receiving VL53L7CX sensor ranging result with status 0 only

Hi all, I'm using pololu VL53L7CX sensor carrier board interfaced with Nucleo-L552zeq EVK for ranging application. For first level, iam using the Simple ranging application that comes with software package. Sensor api calls till getting the data seem...

Aju004 by Associate
  • 1874 Views
  • 4 replies
  • 0 kudos

VL53L4CX Setup Problems / Hard Fault?

Hello, I am having trouble with the VL53L4CX Sensor for my Capstone Design Project. My group created our own breakout board for the sensor, and I was able to get it up and running with the VL53L4CX_SimpleRanging project provided by ST.However, I am h...

cory9_1-1740376058750.png cory9_3-1740376144306.png cory9_4-1740376180798.png cory9_5-1740376201638.png
cory9 by Associate
  • 1577 Views
  • 3 replies
  • 0 kudos

Resolved! Sensor intrinsics for VL53L8CH

I am working with the ST VL53L8CH sensor for research purposes. To generate a point cloud from depth measurements, I am trying to get the directional ray to each zone. I am wondering if there is a more detailed explanation of the configuration for SP...

a.png b.png
wsun by Associate
  • 1110 Views
  • 1 replies
  • 1 kudos

Resolved! Problems with initialization of VL53L1X

Hi, I am looking for a ToF sensor using VL53L1X.We are currently developing a ToF sensor using VL53L1X.I have a question about the sample API VL53L1X_UltraLowPower you are using.Whenever I execute VL53L1X_ULP_CheckForDataReady within VL53L1X_ULP_Sens...

AL_HM_2-1738847675154.png AL_HM_3-1738847737661.png
AL_HM by Associate
  • 2408 Views
  • 2 replies
  • 0 kudos

Resolved! VL53L4CD (ULD) not ranging?

We are moving to VL53L4CD.Have it all coded but having a strange experience.  Simplistically we use the sensor continuously and only use GetResult to retrieve the sensor readings (e.g. not CheckforDataReady).So,  simplistically looks sorta like this ...

will3 by Associate III
  • 1791 Views
  • 2 replies
  • 0 kudos

Resolved! VL53L8CX at 60 Hz

I am trying to run a VL53L8CX sensor at the maximum advertized speed. Originally, following the marketing for this chip, I had thought that this was possible at the full 8x8 sensor resolution, but later learned that that has a maximum speed of 15 Hz ...

256 by Associate II
  • 1984 Views
  • 3 replies
  • 2 kudos

Resolved! VL53L4CD Configuration

static const uint8_t VL53L4CD_DEFAULT_CONFIGURATION[] = {#ifdef VL53L4CD_I2C_FAST_MODE_PLUS0x12, /* 0x2d : set bit 2 and 5 to 1 for fast plus mode (1MHz I2C),else don't touch */#else0x00, /* 0x2d : set bit 2 and 5 to 1 for fast plus mode (1MHz I2C),e...

will3 by Associate III
  • 2741 Views
  • 1 replies
  • 0 kudos