@Federica Bossi Thanks for confirming AN5983 on orientation of the Fresnel Lens. Please note that the Fresnel Lens has a flange (as shown in the illustration in AN5983), which causes the lens to only fit one way in the ST STEVAL-MKI1231KA sensor ev...
@Federica Bossi Can your team resolve the apparent conflicting lens mounting orientation specification between the Fresnel Factory documentation, AN5983 and the sample lens mount included in the ST STEVAL-MKI1231KA sensor evaluation board?
@SLERO.1 @Federica Bossi I too am watching for ST support response to explain the results you are seeing. I suspect the results are being impacted by the setting of the digital filters (Presence and Presence/Motion) but it is unclear how to adjust ...
According to AN5983 (Reference Lens of the STHS34PF80 in the final application), and my own testing, the Fresnel Factory TMOS63-10 lens is to be mounted with the Grooved Surface of the Fresnel Lens mounted away from the STHS34PF80 sensor. However, t...
Per AN5867, section 7.1 Presence Detection. As described and illustrated in Figure 4, as long as PRES_FLAG is true (TPRESENCE exceeds PRESENCE_THS), the output value of the LPF_P filter is fixed. This will affect the value of TPRESENCE once the Pre...