User Activity

Hi,I am using the VL53l8 sensor. i need to change the ranging frequency. im using the Xcube tof code. I see in the app tof code that #define RANGING_FREQUENCY (10U). so if i change 10u to 15. Willi get ranging frequency to 15 hz.? Thank u 
HI,I am using VL53L1 sensor for a custom project. I had some queries regarding the sensor,1) what is the integration time for the SPAD sensor?2) What is the max sampling rate of the SPAD sensor (ADC conversion)? What is the sampling frequency of the ...
Hi,Can somebody please suggest me a ToF sensor with signal sampling rate of atleast 1MhZ. Thank you
HI,I am working on VL53L1 sensor using X CUBE TOF1 software. I want to change the I2C speed to 1MHz. Can somebody guide me how to do it?Thank you
Hi,I am looking to print only the signalrate in MCPS of the VL53L1. What should I do?
Kudos from