GNSS positioning

Ask questions and find answers on Teseo GNSS positioning solutions. Discuss NMEA sentences, SBAS activation, and signal troubleshooting.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Teseo-LIV3F, No GPS coordinate

I made a PCB using Teseo-LIV3F as stand alone, tried to connect TX and RX of the module to Arduino TX and RX using I TinyGps++ library, but I couldn't get any response from the module. I tried to connect the module to software and hardware serial of ...

AAl S.1 by Associate II
  • 3572 Views
  • 13 replies
  • 0 kudos

Teseo LIV3x

Hello,I’m looking into buying a Teseo LIV3x module (one of both). What I saw in the datasheets is that they accept RTCM messages, is that true? Does this mean that if I give the module these messages, it will output corrected nmea sentences?I saw tha...

RVerv.1 by Associate
  • 567 Views
  • 2 replies
  • 0 kudos

Resolved! Hi, I want to connect Teseo-Liv3R to an active antenna. I have seen in the Data sheet section number 6.2 how to connect it. My questions:

1- What is the deference between figure 10 and 11? And what is (S22943) in figure 11? is all I need to use active antenna inductor and capacitor? If it is yes what is the value?2- I have seen in the   in section 7 general schematic. Is it for passive...

AAl S.1 by Associate II
  • 1056 Views
  • 1 replies
  • 0 kudos

Cannot apply a configuration change to binary image

Trying to load a baud rate change config to bin image using wizard and "I want to modify a binary image", then choosing an option to apply to software binary image. The result is is cannot be applied by this wizard. The binary version is BINIMG_4.7.1...

Mark1 by Associate
  • 473 Views
  • 0 replies
  • 0 kudos

Resolved! TESEO-LIV3R EEPROM

Hi, Does TESEO-LIV3R require to connect EEPROM? If it's yes why do we need it? In my application i need to do hot start. Is it just enough to connect V_Back to external battery?Best regards Anas

AAl S.1 by Associate II
  • 628 Views
  • 2 replies
  • 0 kudos

Resolved! where are the STA8089FG IC internal antenna and splitter?

Hi, the user manual of the ST8089FG mentions an internal antenna and splitter but the datasheet does not talk about it, and even if they were external in the ADC hardware reference design the document does not indicates the model of the splitter or t...

0693W000000WZslQAG.jpg 0693W000000WZZZQA4.jpg

Resolved! How to integrate STA8089FGBD and IMU to use DRAW?

Hi, the STA8089FGBD is an GNSS IC that supports DRAW, but it does not integrate an embedded IMU, I want to connect an external IMU to be able to use DRAW, but I cant find any hardware or sofware reference design to achieve this, does anybody have any...

Resolved! TESEO-LIV3F

Hi, I have TESEO-LIV3F , I want to power the GPS when it's needed. I have backup battery connect to VBAT because i want to have hot start . 1- In my case how much current draw from the GPS when only VBAT powered? It says in data sheet 6uA as hardwa...

AAl S.1 by Associate II
  • 921 Views
  • 3 replies
  • 0 kudos

How to enable GPGLL on Teseo-Liv3F module ?

I am working with Teseo-Liv3F to test NMEA0183 strings over BLSP UART 12 on my board.wanted to know how reset and wakeup are used to monitor UART transfers ?How can we enable GPGLL, GPVTG on the module to obtain NMEA strings?To test the antenna used ...

YJain.1 by Associate II
  • 3048 Views
  • 16 replies
  • 0 kudos