2020-06-11 4:59 AM
1- What is the deference between figure 10 and 11? And what is (S22943) in figure 11? is all I need to use active antenna inductor and capacitor? If it is yes what is the value?
2- I have seen in the in section 7 general schematic. Is it for passive antenna only?
Thanks
best regards
Solved! Go to Solution.
2020-06-29 1:44 AM
> What is the deference between figure 10 and 11? And what is (S22943) in figure 11? is all I need to use active antenna inductor and capacitor? If it is yes what is the value?
fig.10 and Fig11 are similar. In the second case (fig.11) the switch works also as current limiter
There is a type in the image S22943 stands for TPS22943.
>2- I have seen in the in section 7 general schematic. Is it for passive antenna only?
Yes.
Regards
Francesco
2020-06-29 1:44 AM
> What is the deference between figure 10 and 11? And what is (S22943) in figure 11? is all I need to use active antenna inductor and capacitor? If it is yes what is the value?
fig.10 and Fig11 are similar. In the second case (fig.11) the switch works also as current limiter
There is a type in the image S22943 stands for TPS22943.
>2- I have seen in the in section 7 general schematic. Is it for passive antenna only?
Yes.
Regards
Francesco