2020-06-21 4:54 PM
Hello,
I’m looking into buying a Teseo LIV3x module (one of both). What I saw in the datasheets is that they accept RTCM messages, is that true? Does this mean that if I give the module these messages, it will output corrected nmea sentences?
I saw that there is a binary which you can flash so that it outputs raw measurement data. So theoretically I should be able to use it with RTKlib?
I was searching for answers on these questions, but can’t find much info on this.
I dont need to make myself a RTK base station, because in my country (Belgium), there is a free service (FLEPOS), which we can use to get NTRIP.
kind regards
Raf
2020-06-21 6:34 PM
>>I saw that there is a binary which you can flash so that it outputs raw measurement data. So theoretically I should be able to use it with RTKlib?
My understanding was that the measurements were very noisy
The RTCM3 would only support DGPS/SBAS type pseudo-range correction as I understand it.
2020-06-29 1:51 AM
Hi
> What I saw in the datasheets is that they accept RTCM messages, is that true
Yes. LIV3F suspport RTCM v2.3
> I saw that there is a binary which you can flash so that it outputs raw measurement data. So theoretically I should be able to use it with RTKlib?
No. You can't.
ST provides pre-builded binary. You can not flash a generic binary. in detail there is no LIV3F binary which provides raw measurement data.
Hope this helps
Regards
Francesco