Subject | Author | Posted | |
---|---|---|---|
Hello, I'm trying to share buffer between files but sometimes I get value sometimes not. And this ...
| 2023-03-15 06:26 AM | ||
Hello, I am facing a glitch issue when the frame buffer is switching with a custom widget. Both ...
| 2023-03-14 05:27 AM | ||
I am facing performance issue due probably to my way for invalidation on data update. I have widget...
| 2023-03-14 03:19 AM | ||
Hi, I'm looking to use a scroll list as a debugging window which records messages to a textarea wi...
| 2023-03-12 08:41 AM | ||
I am trying to make screen (slide) transition smoother using cachable container. I am trigerring sl...
| 2023-03-07 12:30 AM | ||
I use a module which uses C instead of C++. There is a feature used, which is available in C 99 b...
| 2023-03-06 01:47 AM | ||
Hi everyone, I'm doing a game project with ST32 and ToughGFX for my Embedding Course. It's my first...
| 2023-03-05 09:10 AM | ||
I would like to implement a screen timeout feature on our design. At timeout the screen would go ba...
| 2023-03-02 08:37 AM | ||
I want to know the calculations required to figuring out the hardware required to get drive a perti...
| 2023-02-25 11:53 PM | ||
Hi, I've inherited a project which was designed using the STM32F746-G Discovery board as a referen...
| 2023-02-24 04:52 AM | ||
I am currently using Pn532 nfc SPI and lvgl for the display in STM32F469. I am using freertos to ru...
| 2023-02-15 07:53 PM | ||
Hello, I am trying to prepare some code for my custom board that has an LCD-TFT display on it. To ...
| 2023-02-13 11:57 AM | ||
Hi there I'm currently working on a simple project and it is a simple 7inch LCD using a STM32H743I...
| 2023-02-12 03:29 AM | ||
I want to add another dislay(replace another) display with my STM32F7508-DK board which uses differ...
| 2023-02-09 10:18 AM | ||
I using dynamic graph, I set 100 data points. Since a graph reset, the graph change scale by itse...
| 2023-02-06 02:41 AM | ||
This is the basic idea, but now the dual-screen is bricked. Here is a Detail reading link to tha...
| 2023-01-23 10:07 AM | ||
Hey We are trying since a few days to reset our Display after Stop Mode, without much success. We ...
| 2023-01-19 12:14 AM | ||
I am using controller STM32H745BIT6 device with QSPI flash connected. I have configured the Touc...
| 2023-01-18 07:10 AM | ||
Hi, I'm working on a project using DSI to print LCD with STM32F769I-Eval. In this kit, there is a ...
| 2023-01-18 12:25 AM | ||
< /* Initialize all configured peripherals */ MX_GPIO_Init(); MX_I2C1_Init(); /* USER CODE ...
| 2023-01-09 01:37 AM |