Subject | Author | Posted | |
---|---|---|---|
Hi, I'm currently working on the STM32H753I-EVAL02 with the 5.7" parallel RGB 24 screen. Now, I...
| 2022-12-12 02:43 AM | ||
2022-12-09 02:27 AM | |||
Hi, I am trying to add files from an external library to be build and executed with the TouchGFX...
| 2022-12-03 08:30 AM | ||
Hi everyone, The text translation functionality of TouchGFX is awesome and implemented easily by j...
| 2022-12-01 06:24 AM | ||
Currently I am using TouchGFX 4.20 I created Project, I am able to configure USB as CDC by Adding #...
| 2022-11-28 01:30 AM | ||
Hi, I want to know ,Is it possible to customize vertical font line in dynamic graphs... instead of ...
| 2022-11-21 12:39 AM | ||
Has anybody project for board STM32F469i and display 800x480 with NT35510 controller ? I tried r...
| 2022-11-17 11:34 PM | ||
Hi all, I am currently using the STM32F769-Discovery board. I am looking to display a GUI de...
| 2022-11-14 07:04 AM | ||
Hello, The image attached should display 4 times the same .png image. The top line (left = .png...
| 2022-11-09 12:39 PM | ||
We are working on camera live streaming project. here we have achieved raw bayer to argb conevrtion...
| 2022-11-08 09:01 PM | ||
can i use stm32 hal libraray to interact touch gfx with hardware without using task and queue metho...
| 2022-11-07 08:53 PM | ||
2022-11-03 11:28 AM | |||
Hi, I am working on a TouchGFX project, which connects my STM32F429IIT6 with a custom board with 2...
| 2022-11-03 01:49 AM | ||
Hi everyone I am looking for a solution about designing a multi-language keyboard on TouchGFX usin...
| 2022-10-24 08:02 AM | ||
Hello, My question would be the same as on top of this post. So far i was not able to do it. I kno...
| 2022-10-23 10:55 AM | ||
Hello, I've followed the example given in the link below in order to call the screen from the co...
| 2022-10-12 02:34 AM | ||
Hi Community, How to store Video (.obj and .bin) files in external memory as they have stored in...
| 2022-10-06 11:50 PM | ||
AFAIK, destructors are meant for "deinitialization", freeing memory and such. But isn't it what tea...
| 2022-10-02 12:27 AM | ||
I am trying to export a project from Storyboard to Cube IDE. I have seen a few tutorials through IA...
| 2022-09-28 10:09 AM | ||
Hi all, Gfx can generate L8_RGB565 & L8_ARGB8888 format bitmap, but each pixel retains one byt...
| 2022-09-27 09:00 PM |