| Subject | Author | Posted | |
|---|---|---|---|
|
I am using STM32CubeH7 from GitHub (the latest commit is here). In stm32h7xx_hal_nand.c, I found so...
| 2024-09-09 5:05 AM | ||
|
As I am working on the stm32G474VETx with LQFP100 packing. For master and slave, I am using same ty...
| 2024-09-04 1:32 AM | ||
|
I am using stm32f4 for lwip ethernet It works nice with my custom monitoring program, hercules ...
| 2024-09-03 9:35 PM | ||
|
@Erwan SZYMANSKI I am trying to establish SPI communication between two STM boards: the Nucleo G4...
| 2024-09-03 6:05 AM | ||
|
I have a project using all custom code (not HAL) in which I have two 6 byte SPI DMA transactions ru...
| 2024-08-28 1:24 PM | ||
|
Hi As i am using one of TIM8 input for external BKIN pin, to detect fault for PWM shutdwon. But ...
| 2024-08-23 1:10 AM | ||
|
Regarding the KNX TP, I tested the STKNX evaluation board and my board which have ST-KNX chip then ...
| 2024-08-20 4:25 AM | ||
|
Hi everyone, I'm working on decoding an SBUS signal, which uses an inverted normal UART protocol, ...
| 2024-08-18 8:26 AM | ||
|
Hi,
I have ported the Open Bootloader to the STM32G431 and has flashed it and is able to communic...
| 2024-08-14 5:33 AM | ||
|
Well, I'm developing a system for reading sensors and sending them to a server. I'm using a GSM LT...
| 2024-08-13 8:45 AM | ||
|
I've successfully set up an evaluation project on the STM32U5A9J-DK PCB with a custom 640x480 MIPI/...
| 2024-08-13 7:34 AM | ||
|
I'm currently testing low-power applications on the NUCLEO-U545RE-Q board, which involves using an ...
| 2024-08-13 12:32 AM | ||
|
Hi, I'm using the software EEPROM to save a variable to flash that is being updated during run tim...
| 2024-08-12 5:40 PM | ||
|
I am trying to implement an IAP function on stm32h563 with Keil. I have a bootloader and image A an...
| 2024-08-12 3:41 PM | ||
|
Hello, SDIO 4 bit R/W with 32 bit HC works. When 64 GB XC is used getting error at: SD_PowerON() ...
| 2024-08-12 6:26 AM | ||
|
Hi, I am very new to the matter protocol and seeking to implement a matter protocol for STM32 NUCL...
| 2024-08-11 10:42 PM | ||
|
I am trying to flash and debug my .elf file with the help of openocd and gdb server in UBUNTU . Aft...
| 2024-08-11 11:02 AM | ||
|
Hi there, I am writing a custom video decoding app that process custom stream JPEG frames from USB,...
| 2024-07-30 6:16 AM | ||
|
If you enable Transmission Complete (TC) interrupt flag TCIE in the UART_CR1 register before enabli...
| 2024-07-30 1:30 AM | ||
|
I made a board with spi1 connect a lora module, and the nss pin, I just want to use soft control. B...
| 2024-07-29 4:52 AM |