| Subject | Author | Posted | |
|---|---|---|---|
|
If you enable Transmission Complete (TC) interrupt flag TCIE in the UART_CR1 register before enabli...
| 2024-07-30 1:30 AM | ||
|
I made a board with spi1 connect a lora module, and the nss pin, I just want to use soft control. B...
| 2024-07-29 4:52 AM | ||
|
Hi all, Currently I am working on a project using STM32U575ZG with both ADC1 and ADC4 enable. 1...
| 2024-07-25 7:10 AM | ||
|
I am working with an STM32F405 and have the I2C1 peripheral set up as a master in standard mode wit...
| 2024-07-25 6:50 AM | ||
|
Good day, Hope you're well. I used CubeMX to setup a PWM timer on the STM32F3 discovery board and ...
| 2024-07-24 7:26 PM | ||
|
Hello, We are using STM32L412RBT6 MCU for our inverter and battery charger application. We are ...
| 2024-07-24 3:33 AM | ||
|
Hello, I have a code snippet where I initialize PSP (stack pointer) to its very first location, an...
| 2024-07-23 11:36 PM | ||
|
Hi everyone, I'm new to STM32. I'm trying to use the STM32C011x4's internal temperature sensor. I'...
| 2024-07-22 12:58 PM | ||
|
Any suggestions as to why power down, then reconnect debugger (JLINK pro) is clearing the ...
| 2024-07-22 8:16 AM | ||
|
I generated a project using STM32CubeMX, in which I tried to use SDIO and FatFS. However, it doesn...
| 2024-07-20 11:46 PM | ||
|
NUCLEO-F030R8 does not appear in FINDER on Mac
Also the option is missing from list of ports
Ha...
| 2024-07-19 4:13 PM | ||
|
Dear Community. Short Rant (sorry, need to let off some steam): I wonder, why there is not more q...
| 2024-07-17 10:16 AM | ||
|
Hi I'm designing a PCB using the STM32H735 based on the eval kit STM32H735G-DK. On STM32H735G-DK ...
| 2024-07-17 1:19 AM | ||
|
This is new. I've used it in the past and downloaded data with no problem. Yes, I do have netw...
| 2024-07-16 11:53 AM | ||
|
Previously, I had a Raspberry Pi CM4 connected to an existing WebSockets server developed with Djan...
| 2024-07-16 8:38 AM | ||
|
Hello, I have been working on the STM32G030K6T6 with DMX512 and TM1651 display for 8 months, and I ...
| 2024-07-16 5:26 AM | ||
|
Hi everyone, 1, What are the acceptable buffer sizes for the DFSDM PDM mic configuration, give me ...
| 2024-07-15 11:55 PM | ||
|
Hi, I am unable to communicate via i2c with the TLV320AIC3104IRHBR chip, the bus response is always...
| 2024-07-15 2:20 PM | ||
|
Hi there, Iam able to send data to external DAC with SPI DMA timer update on the SPI-2, the proces...
| 2024-07-10 8:59 PM | ||
|
Hello, the reference manual of the STM32G4 Series states, concerning the arbitration of mem2mem tr...
| 2024-07-08 7:55 AM |