| Subject | Author | Posted | |
|---|---|---|---|
|
Hello I'm developing RTOS environment of dual-core in STM32H757. In OpenAMP communication mode...
| 2024-10-20 7:18 PM | ||
|
Hi. First time using this forum. I'm using an STM32F103C8 (genuine, not bluepill clone). I've eas...
| 2024-10-20 3:31 AM | ||
|
Hi everyone! I have this code where the mcu goes into STOP3 mode, and is waked up by a button trig...
| 2024-10-14 3:22 PM | ||
|
Dear Team, We are using the STM32G473VET6 microcontroller with the IMP34DT05TR microphone, uti...
| 2024-10-10 6:28 AM | ||
|
I redid FatFS to work async or in polling mode. Works well on my STM32H755zi, on CM4. Most function...
| 2024-10-09 8:04 AM | ||
|
Hello, I am trying to integrate internet connectivity on the STM32F407 using an LTE modem via the ...
| 2024-10-08 8:37 AM | ||
|
Hi. I am using the STM32H7S78-DK board. In STM32CubeIDE, I checked the example for jpeg_encodi...
| 2024-10-02 12:19 AM | ||
|
We tried to set the OP bytes using the JLink.exe through command line. We tried to enable TZEN and ...
| 2024-10-01 5:40 AM | ||
|
I'm having difficulty writing to STGAP1BS configuration registers. I'm using a Nucleo -G474RE to ...
| 2024-09-26 10:14 AM | ||
|
Hello Community, We have issues with a STM32F407G-DISC1 board. We had the board running in our ca...
| 2024-09-18 9:14 PM | ||
|
Hello, Hello, I am seeking either a ready-to-use or partially implemented driver for the HM01B0 ...
| 2024-09-18 7:57 AM | ||
|
Hi, i start design on G4 and am confused with internal ref in MX. 1. Internal REF for ADC isnt rea...
| 2024-09-18 1:17 AM | ||
|
I am developing a application for Battery based 4G GATEWAY so most of the time I want my micro-cont...
| 2024-09-17 4:49 AM | ||
|
Hello,
I wanted to have SPI with DMA RX, below issues I face:
1. When SPI RX DMA function used...
| 2024-09-15 10:07 PM | ||
|
Hi, I'm trying to apply an Offset on the ADC, I'm using a H743. I'm pretty sure I have the ADC wor...
| 2024-09-15 1:07 PM | ||
|
Hi. I'm trying to configure a wake-up alarm (Alarm A) to wake up (for a test) after 5 minutes, bei...
| 2024-09-13 12:56 PM | ||
|
Hi everyone, long story short is that i'm trying to use the system bootloader capabilities to handl...
| 2024-09-13 1:17 AM | ||
|
Hello, I am using RTC internal wake [10 sec] using the following code: void go_to_sleep(void)
{
...
| 2024-09-12 11:44 PM | ||
|
Hello. In STM32H7S7L8HXH_flash_default_app.ld, it is set to __FLASH_BEGIN = 0x08000000, In STM3...
| 2024-09-12 10:25 PM | ||
|
Hi, the platform is STM32U57X Question: The variable is in the non secure area of SRAM. Why can...
| 2024-09-12 4:30 PM |