Same or related posts https://community.st.com/t5/stm32-mpus-products/op-tee-error-on-new-v5-0-0-sdk/td-p/578239/page/2 https://community.st.com/t5/stm32-mpus-products/op-tee-error-tzc-permission-f...
Hi everybody, I'm trying to configure the Wi-Fi module on my custom board (based on the STM32MP153, the Wi-Fi module already tested OK) in Access point mode, and I found the official guide to ...
I'm trying to get to know stm32mp1 while making a board for this thing. While using the default image provided by manufacturer seems to work. The kernel used is old compared to the current ST BSP an...
I downloaded the STM32MP151AAC3 example model (.zip file) that routes traces to the DDR3L memory STM32MP151A - MPU with Arm Cortex-A7 650 MHz, Arm Cortex-M4 real-time coprocessor, TFT display - STMi...
I want to connect AWS IoT on STM32mp135f-dk board. so, I install pkg sudo apt-get install git sudo apt-get install cmake sudo apt-get install build-essential but, can't auto install buil...
Hi, I am trying to create an image for writing to NAND memory. The problem is that when generating a TSV file using Yocto, I get a layout without a bootfs partition. In this case, it is u...
I'm trying to testing secure boot on a STM32MP157F-EV1. To do so, I planned to use the fuse override command to test secure boot without having to actually burn the OTP 24-31 with the public key h...
Hi there, I am working on an STM32MP157F-DK2 board and an STUSB1600 with hsotg gadget support and no PD controller. I am running a buildroot image with all the necessary drivers enabled incl...
Hello I tried everything but I cannot get STM32CubeIDE to get the editor to work. I just keep on getting this message: There is no active editor that provides an outline. I spent hours re-installi...