Hello, Introduction I would like to profile a motor which is not in the motors tab in MC Workbench. I have done some Googling and reviewed the ST documentation (STM32 Motor Control SDK > Mo...
Hi there, I recently purchased the B-G431B-ESC1 and when I connect it to my USB port, immediately a red flashing light appears. There are two other solid green lights. I am als...
Hello there, I am new to the MC Workbench and must configure the B-G431B-ESC1 to use it with a A2212/6T 2200KV Brushless DC Motor. I created a new project in the MC Workbench 6.3.0 a...
I am trying to generate code for "STM32 Nucleo packs FOC and 6-step motor control platform for three-phase, low-voltage and low-current motor" and I keep getting errors :- Attr not supported : Dmpu&...
[VERSION]: MCSDK 6.2.0 [TOOL]: MC Workbench [DETAILS]: Hi I want to prototype the HSO algorithm to compare the performance with the current Observer. From a webinar I have ...
The P-NUCLEO-IHM03 with type selected as "FOC" has the firmware pre-installed. After pushing Blue start/stop button, the motor starts but fails to continue.
In Motor pilot, it is showing that a fau...
Hi everybody, First of all I don't have experience in FOC. I have profiled the motor, and the procedure was succesfully completed. I use the motor profile to create a FOC project. When I try to s...
Where to find user manual UM3118 referenced in B-G473E-ZEST1S Data Brief. The link to this manual in the data brief goes to Page Not Found. Many thanks.
Hi, I am trying to understand the protocol, especially how to interpret the data packets to have custom code for auto motor ramp-up. I see there are some documents under MC workbench -> About. H...
Hello, I am using the STSPIN32G4 IOC file from MC Workbench for a motor control example. However, I encounter the following errors during the build process. Since these files are auto-generated, I c...