I have this working keras model: https://www.dropbox.com/scl/fi/544ma5tsndw3cjv8djem0/model.keras?rlkey=87845alu8vki9y81kb7tjgrab&dl=1 and I am trying to load it into X-CUBE-AI 8.1.0&nb...
The error occurs when I try to run the code generated for model squeezenetv1.1_xxx_tfs_int8.tflite The command I used to generate code is stm32ai generate -m squeezenetv1.1_128_tfs_i...
so, i have been using nano edge ai since a long time. but now i cannot log the signals when i am trying to. will they be any reason for that. please, solve this.
Hi, I have an STM32H573I-DK Discovery kit with me. I wanted to try out Edge AI applications on it, and was checking out the STM32Cube.AI Developer Cloud. When I reached the "Generate" section and br...
hello, Now I'm trying to implement ML library created by NanoEdgeAI Studio to our STM32C0 target board. My anomaly detection ML looks work fine at this time, but I wonder that every time after boot...
Board - B-L4S5I-IOT01A Board AI application tool - NanoEdge AI Studio CUBEMX IDE - STM32CubeIDE 1.15.1 I made one model. Model detect anomaly on nano studio. I deploy model. Deployed system alw...
To STM, Subject: NanoEdge AI package not compile with B-L4S5I-IOT01A Board. Board - B-L4S5I-IOT01A Board AI application tool - NanoEdge AI Studio CUBEMX IDE - STM32Cube...
Hello, I'm trying to figure out how Unico calculates it feature values during .arff creation. Unfortunately, if I calculate the features as described in AN5804, the feature values differ from the U...
Hello everyone, I am working on a project using nanoedge studio ia in rating N, I want to check my project with cube ide, I can make a view with tera term or other tool, which shows the result corres...