User Activity

Hi,I'm working on a hardware design using the STM32F765VIH and I am trying to connect a MT28EW128ABA1HPC-0SIT NOR Flash and IS66WVH16M8DBLL-100B1LI PSRAM to the FMC in muxed mode. I'm struggling to understand how the muxed connection should be made a...
I have this working keras model: https://www.dropbox.com/scl/fi/544ma5tsndw3cjv8djem0/model.keras?rlkey=87845alu8vki9y81kb7tjgrab&dl=1 and I am trying to load it into X-CUBE-AI 8.1.0  When I hit Analyze I get this error: Neural Network Tools for STM3...
I have a custom design using the S2-LP and SE2435L amplifier, largely similar to the STEVAL-FKI915V1. About one year ago we produced a first batch of prototypes and it all worked perfectly on the Sigfox side. Now I am testing a second version prototy...
Hi,I have a custom design based on the S2-LP eval kit, tested my firmware (based on the ST Sigfox Library) with the eval kit and ST's ID/PAC and all is working fine. Custom hardware is also working fine and now I am in the process of installing the p...
Posted on January 16, 2017 at 16:16I've noticed that in the STM8S standard peripheral libraries, in the UART1_Init function there is an assertion checking the baud setting:assert_param(IS_UART1_BAUDRATE_OK(BaudRate));Digging into stm8_uart1.h, the d...
Kudos from
Kudos given to