cancel
Showing results for 
Search instead for 
Did you mean: 

X-Cube-AI encounter problem while model check

WeslyDreamer
Associate

Hi,

 We put our network onnx into X-Cube-AI but it is not pass the test. it shows the following error message:
 
Analyzing model.:/Users/DELL/STM32Cube/Repository/Packs/STMicroelectronics/x-CuBE-Al/9.0. 0/Utilities/windows/stedgeai.exe analyze -target stm32h7 -name network2-mC:/Users/DELL/Desktop/mathfunction model 1.onnx--compression none--verbosity1allocate-inputs --allocate-outputs --workspace c:/Users/DElL/ApData/Local/Temp/mAI workspace2837949619220009026241954990433454utput C:/Users/DELL/.stm32cubemx/network outputSTEdgeAl Core v9.0.0-19802
TOOL ERROR:tuple index out of range

So how to fix this error?
Thanks!
Here is the  network structure.

eb5989831fcff215753695441f60f7d.png

1 REPLY 1
Julian E.
ST Employee

Hello @WeslyDreamer ,

There was an issue with the Gather, please use the latest available version of X-Cube-AI.

You can also set the environment variable  _DEBUG=2 and post your error if you still have one.

 

Have a good day.

Julian


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.