cancel
Showing results for 
Search instead for 
Did you mean: 

FP-IND-PREDMNT1 wi-fi connection error

bcryhun
Associate II

Hello I have STEVAL-STWINKT1B device. When i try to connect wifi with tera term it gives this error:

platform_init L#234 The network interface can not be started

any advice?

3 REPLIES 3
niccolò
ST Employee

Hi @bcryhun ,

it may depend on the firmware installed on the STWIN. can you check which is it?
this is the first I would try to work with WiFi:  FP-AI-PREDMNT2 

If this answers your question, please, mark this as "best answer", by clicking on the "accept as solution" to help the other users of the community

Niccolò

bcryhun
Associate II

i did use fp-ai-predmnt2 and follow steps on documentation. It is same, i can not connect to wifi. When i try to write ssid and password, it does not give any response

Hi @bcryhun ,

what toolchain did you use?
were you able to check with debug if the fw has some problem somewhere?
if you tell me where it gets stuck I can try to help you overcoming this issue

Niccolò