Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! SPC560P50L5 & MPC560

I am using SPC560P50L5 microcontroller.Can I code with MPC560 microcontrollers and CodeWarriorIDE software and transfer the hex file to SPC560P50L5 microcontroller???

Resolved! SPC56XX JTAG Password Send Sequence

I have a SPC56XX part which I need to unlock for a JTAG OnCE debug session.The procedure for enabling debug on a locked device is described in AN4035, however when I follow the steps I get no response from the MCU when sending correct password. Is th...

tbnkr by Associate II
  • 3190 Views
  • 2 replies
  • 0 kudos

Resolved! SPC5 Motor Control Live Monitor location?

​Hello ST Community,​Documentation for the Motor Control Toolkit and L9907 often reference a SPC5 Motor Control Live Monitor. Is the Live Monitor still downloadable from somewhere, even if we have not bought the kit with a motor, L9907 and SPC560P? T...

EPelt.1 by Associate II
  • 4614 Views
  • 8 replies
  • 0 kudos

In the watch dog windowed mode the service routine causes an unhandled exception unless the countdown timer is less than the SWT_WN register.

 However the countdown timer SWT_CO cannot be checked unless the watchdog is disabled. Is there a way check the countdown timer without disabling the watchdog timer. Or is it OK to disable the watchdog timer check the countdown timer the enable the ...

CGilm.1 by Associate
  • 1234 Views
  • 1 replies
  • 0 kudos

SPC582B60E1 CAN message filtering issue.

I am using dedicated Rx buffer and configured the filter to accept 3 CAN messages.For example,0x250 in Rx buffer 00x240 in Rx buffer 70x270 in Rx buffer 12Total number of Rx buffer used 32.Using MCAN Subsystem 0 MCAN 0. Shared RAM size is 3072. Stand...

DKuma.3 by Associate II
  • 1441 Views
  • 1 replies
  • 0 kudos

Resolved! Incoherence in clock tree for SPC582 in SPC5Studio

Hello,I found unexpected behaviour in clock tree: when I change CGM_SC_DC2 divider - it affects another line in the diagram (the one with "FBRIDGE_CLK"). And when I change CMG_SC_DC3 divider - it affects the line above ("PBRIDGE_CLK").Best,Yannek

0693W000001qeTQQAY.png
Yannek by Associate III
  • 4224 Views
  • 7 replies
  • 1 kudos

SPC58XXADPT100S Hardware User Manual and Schematics

Hello,Could someone from ST side provide these two documents for the SPC58XXXADP100S minimodule? I have only the documents for 64 Pins and found there are some small hardware differences for the 100S. (Some Jumpers which are not mentioned in the doc...

bgong by Associate
  • 1241 Views
  • 1 replies
  • 0 kudos