User Activity

Hi I am developing my project using the SPC58EC74 chip,I found two problems when using SPI(The clock I/O is PG[11]/DSPI0_SCK, which is pin 34)。first question:When the amount of my code is relatively small, the clock signal is normal; when the amount ...
Hi, I am currently using the SPC58EC series of microcontrollers. I would like to know, for an I/O (configured in input mode), at what input voltage level it will be recognized as a high level. Is this voltage value configurable? Thank you for your re...
Hi,   I'm learning to use it SPC58EC serial chip and have a question,when it was previously used on Arm chips, there were some exception handling interrupt functions,like Hard_Fault_Handle,this ensures easy traceability when problems arise, my questi...