Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Error encountered while building the code

./components/spc574sxx_low_level_drivers_component_rla/lib/include/spi_lld.h:690:2: error: #error "SPI driver activated but no DSPI peripheral assigned"#error "SPI driver activated but no DSPI peripheral assigned" This is the error i encountered whil...

SPC5 GTM Cluster Clock issues

Using the SPC572Lxx RLA GTM DPLL Test Application for Discovery all works fine until for some reason the Cluster Clocks in the Clock Manager Unit of the GTM IP Configuration changes to what´s shown in the picture and we get the Error "2' is not a val...

Larsa by Associate III
  • 1583 Views
  • 0 replies
  • 0 kudos

FDA903D unable to play audio out on custom hardware

Hello All, We have designed our own custom hardware using SPC582bxx automotive controller and FDA903D audio amplifier. We built the code test the audio amplifier, code is very simple to play audio. We have used SPC582Bxx Engine simulator code and mod...

Resolved! SPC58EC80 CanBus RTR Frame Request

I'm using SPC58 DISP Board for RTR request data frame from a battery pack. I have set the RTR value as 1, but didn't receive any reponse data frame from the battery. I have tested with CAN analyser, reponse data frame is coming(working fine). When I ...

Screenshot 2024-06-19 185331.png

Resolved! Reference Design

I am MURAL SELVAM from India. I am Currently working on Automotive project I need reference Design for Below given part number..SPC560D30L1B4E0XIf You have any reference design kindly provide me.

murali by Associate III
  • 1905 Views
  • 1 replies
  • 0 kudos

CAN1/2 DMAMUX on SPC58 2B

Hello,Looking through the reference manual for this chip on page 111 (RM0403 R7) it looks like there is a DMA peripheral line from CAN 1 and CAN 2 to the DMA module. I can't seem to find any reference to this on the MCAN side though or how to enable...

OHarc.1 by Associate II
  • 1712 Views
  • 2 replies
  • 0 kudos

Overwriting on chip EEPROM issue

HelloI'm working with spc560p40 and using it's on chip EEPROM. Everything is ok with writing data in any ID, but when I want to overwrite any ID that filled before, the MCU will stop. Its ok for one time writing but for second time writing and more, ...

DNewm.1 by Associate III
  • 1590 Views
  • 1 replies
  • 0 kudos

SPC58ECxx-DIS CANFD with DMA

I want to use DMA to transfer messages received from CAN. However, there seems to be no information in the datasheet about this feature, except for the illustration below. According to this image, it seems like using DMA for CAN is a default feature....

Capture.PNG
tuananh13 by Associate II
  • 1201 Views
  • 1 replies
  • 0 kudos