2014-08-07 3:03 AM
Hello community,
i try to use the PinMap wizard in SPC5 Studio 3 and i receive the meassage ''Device specific model ''SPC563M64L7'' not supported!'' and it seems that there is no support for any model cause i try it with different cpu's. I use the SPC56M- Discovery board and i'm wondering also that this board is not available in the SPC5Studio Application Wizard. Any ideas? Thanks for your help! - MarcSolved! Go to Solution.
2014-09-05 6:39 AM
Hello Marc ,
the pinmap SPC563M64L7 is ready and is available by update site.You can install it from the web by using the command ''Install new software'' Best Regards Erwan2014-08-07 4:34 AM
2014-08-12 2:25 AM
Thanks a lot for the quick answer!
2014-09-05 6:39 AM
Hello Marc ,
the pinmap SPC563M64L7 is ready and is available by update site.You can install it from the web by using the command ''Install new software'' Best Regards Erwan2024-05-24 6:56 PM
Error: flash driver 'spc563mxx' not found