Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Wakeup signal

Posted on May 18, 2015 at 11:05Hello,I am trying to configure a wakeup signal WKPU6 as below.WKUP.WISR.B.EIF = 0x02000000; //Clear interrupt flagWKUP.WIREER.B.IREE = 0x02000000; //Disable rising edgeWKUP.WIFEER.B.IFEE = 0x02000000; //Enable falling ...

ssk by Associate II
  • 1540 Views
  • 2 replies
  • 0 kudos

Resolved! Monaco Pin Assignment_PA

Posted on May 08, 2015 at 04:52Hi. while I am reading SIU PCRxx for Pin Assignment in RM0015 SPC563Mxx Reference Manual, It is not clearly described about Pin Assignment PA[2:0] value. eg. SIU_PCR179. what is value of PA[2:0] for each function of eM...

270284440 by Associate III
  • 1048 Views
  • 1 replies
  • 0 kudos

FlexCAN filter duplicated on all configurations

Posted on May 12, 2015 at 14:11Hello, I'm using both FlexCAN of SPC56EL60 on SPC5 Studio 3.4.3 and I wanted to define filters for each of them. I created a config for each of them containing different filters. CAN1 has 16 filters from 0x200 to 0x20F...

PWM configuration structure

Posted on April 03, 2015 at 08:01I am using SPC560D40L3 with SPC5Studio. I am trying to generate a PWM signal. Using Application configuration, I configured the HAL drivers to generate a PWM of 5Hz. Here, I configured the clock frequency and period ...

ssk by Associate II
  • 2680 Views
  • 7 replies
  • 0 kudos

Application Import - file system

Posted on May 12, 2015 at 08:38I am trying to import settings/files from another project to current project. I followed the steps as File->Import->General->File System and provide the path for source project and click finish. Tool is giving an error...

ssk by Associate II
  • 1890 Views
  • 3 replies
  • 0 kudos

[solved] SPI slave configuration for SPC56EL

Posted on March 26, 2015 at 10:17Hello, I would like to implement a SPI communication between an SPC560D and an SPC56EL Discovery Board. The SPC56EL should act as slave, the SPC560D as master. For both boards, I am using the corresponding DSPI examp...

Patriks by Senior
  • 3223 Views
  • 9 replies
  • 0 kudos

make: *** No rule to make target `all'. Stop.

Posted on April 30, 2015 at 15:17got errors compiling all projects created by wizard:**** Build of configuration Default for project SPC56ELxx OS-Less Test Application for DiscoveryPlus ****make -j2 all make: *** No rule to make target `all'.  Stop....

oleg2399 by Associate
  • 2238 Views
  • 3 replies
  • 0 kudos

Bug on Pinmap in SPC560B50L5 for set PWM

Posted on April 23, 2015 at 10:11Hi I want to Emios-0 in SPC560B50L5 these Specific Pin (PB[11],PB[12],PB[13]) but when i set these pin in pin map as output like E0UC4 or E0UC5 ,... the pin map set the ANX Pins . and i check in spcstudio for use th...

SPC560D30L3 - Serial driver

Posted on March 17, 2015 at 16:11Hello,I am trying to use the serial driver for SPC560D30L3 device using Discovery kit (I have replaced SPC560D40 with SPC560D30 MCU). When I try to configure the 'Serial Driver Settings' for buffer size, it only acce...

ssk by Associate II
  • 2048 Views
  • 9 replies
  • 0 kudos