Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

SPC570S Schematic Symbol & Layout Footprint Available?

Posted on May 23, 2018 at 17:29I'm creating a new project with the SPC570S family and would rather not have to recreate the schematic symbol or layout footprint. They exist, since ST provides an Eval Board. Is there a way to get them to keep from ha...

Resolved! FCCU Exception from MEMU

Posted on May 22, 2018 at 13:47HI,I found an FCCU exception while running some code in Stop mode in SPC58NE84C3(6M). The source for the FCCU is from MEMU(MEMU_RAM_UCE_22)  but i do not know why this error is occurring. Since i'm using Isystem IC5500...

spc560p can abort mechanism

Posted on May 10, 2018 at 13:14hello guys:      I am using the flexcan module of spc560p, now I want to use the abort mechanism to recover the can bus from busoff state by software instead of by the hardware automaticly,because the  hardware rec...

SPC560B Discovery board , Issue with stop mode .

Posted on May 10, 2018 at 06:58I am using spc560b discovery board , i want to implement low power modes like halt , stop and standby ,i am able to implement standby mode and waking up with CAN Rx at PB1 , however when i try with stop modei think it ...

Resolved! Differences between STM32 and SPC5

Posted on April 13, 2018 at 09:23Goodmorning    I'm a newcomer to the microcontrollers of the ST. Until now I have only done some small project with the STM32 family.In these days I'm starting a new project, a control board for a high power outdoor ...

SPC560B-DIS , watch dog issue in debug mode .

Posted on April 06, 2018 at 12:20I am using SPC560B-DIS  discovery board and UDE STK 4.8  debugger for my project .I am facing issue with watchdog during debugging  , i have set my watchdog in window modewith time out period of 100 ms , and window a...

K2 GTM tom0 driver issue based on Studio 5.7.2

Posted on April 04, 2018 at 06:45I tested K2 GTM tom0 channel based on studio version 5.7.2.for example ,tom0 ch0 output 20khz,50% ouput on io port selected in pin  -> it is OK,if I configure tom0_ch0,ch1,ch2,ch3 with same frequence and duty ,and ou...

270284440 by Associate III
  • 1507 Views
  • 2 replies
  • 0 kudos

SPC574 CAN Problem

Posted on March 07, 2018 at 09:14I'm using SPC574K72E5 for CAN application, so I create a demo project SPC574Kxx_RLA CAN Test Application for Discovery and get nothing on CAN output. I have already choose the NO_LOOPBACK mode and select RX/TX pin in...

SPC5-UDESTK or SPC5-UDEDEBG?

Posted on March 27, 2017 at 09:58Hi all, I started with the spc560, I should choose http://www.mouser.vn/ProductDetail/STMicroelectronics/SPC5-UDESTK-EVAL/?qs=sGAEpiMZZMt%2fq2okS0SEEYfDUH7ON2OI or http://www.mouser.vn/ProductDetail/STMicroelectronic...

How to download UDE STK

Posted on April 03, 2018 at 05:28Hello?        Why do I need to download UDE STK correctly after I open the webpage and why don't I download the button?#how-to-download-ude

0690X00000604XmQAI.jpg
Lu Yan by Associate II
  • 1436 Views
  • 1 replies
  • 0 kudos