AutoDevKit Ecosystem

Ask questions and find answers on the AutoDevKit solution. Discuss voltage configurations, motor control, and AutoDevKitStudio programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! AEK-POW-BMS63EN as a Master Board in the daisy chain

Hi,I would like to check if STM AEK-POW-BMS63EN board can be used as a first board in the daisy chain with the setup where we have external MCU (for example STMF103RB) and AEK-COM-ISOSPI1?In the datasheet you describe difference between 'Master' and ...

MaraLo_0-1708798358615.png MaraLo_2-1708798811017.png
MaraLo by Associate II
  • 1068 Views
  • 1 replies
  • 0 kudos

Errata label mismatch on AEK-POW-SPSB081

Dear community members, In the AEK-POW-SPSB081 board, the SPI pin labels (red box in the below image) are not matching the labels of the test points. The correct labels are those placed on the test points (green box).   Thank you for your contributi...

MaxVIZZINI_0-1708777709351.png

Resolved! UDESTK NRND

"Hi,We are building hardware with the SPC58EG80E5 MCU. For debugging purposes, we plan to use the UDESTK-EVAL kit. However, on the product page, it states that it is "not recommended for new designs." What alternative options can we consider?"

cumuk by Associate
  • 2130 Views
  • 2 replies
  • 0 kudos

Resolved! L9663

Hi, I am using L9663, can you send me a driver code? Or a schematic diagram of the wiring

JL1 by Associate II
  • 1809 Views
  • 1 replies
  • 0 kudos

Resolved! L9963E SPI message definition

Hi,I'm trying to understand SPI communication for your L9963E.In the data sheet for your L9963E IC is missing the definition of how SPI shall be configured. It doesn't say anything about MSB/LSB bit send configuration for SPI. In the picture below we...

MaraLo_0-1708370925442.png
MaraLo by Associate II
  • 2234 Views
  • 5 replies
  • 0 kudos

Resolved! 'SPC584B-DISP hardware files

Where can i find the pcb file or gerber file for the SPC584B-DISP, I have a short circuit on board and would like to trace and troubleshoot the board , but i need the hardware files to see where the traces goes to instead of manually looking for it .

kqtay by Associate
  • 1217 Views
  • 1 replies
  • 0 kudos

Resolved! BMS63EN Example does not start

I imported the SPC58EC - AEK_POW_BMS63EN_SOC_Estimation_Single application, configured like described in UM3185. (Side note: The Board View may also view that the ISO SPI needs a Powersupply... So I wonder the Generic pins table..shall I do something...

Orbiter by Senior
  • 4420 Views
  • 4 replies
  • 0 kudos