AutoDevKit Ecosystem

Ask questions and find answers on the AutoDevKit solution. Discuss voltage configurations, motor control, and AutoDevKitStudio programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How can I connect Lauterbach debugger to AEK-COM-10BASET?

Hello support team, I just received a new AEK-COM-10BASET board and trying to connect Lauterbach debugger with License module for MPC55xx. Question : How can I connect to the board through Lauterbach debugger & SW? Currently the SW (TRACE32) shows er...

apap_2-1777512866787.png apap_3-1777512975847.png apap_4-1777513103738.png
apap by Associate II
  • 102 Views
  • 2 replies
  • 0 kudos

Resolved! Cannot start AEK-COM-10BASET project from AutoDevKit 2.7

Hello,   I installed AutoDevKit Studio today and trying to create the AEK-COM-10BASET project from it.   Basically there is no option to create / start the AEK-COM-10BASET from AutoDevKit.   Also I tried to run Help > Install New Software > Work with...

1.jpg 2.jpg 3.jpg
apap by Associate II
  • 211 Views
  • 1 replies
  • 0 kudos

printf() error in AUTODEVKITSTUDIO

Hello Max VIZZINI,i'm facing issue in printf() in AUTODEVKITSTUDIO. im using printf() in the code after compiling im getting this error c:/autodevkitstudio-2.7.0/eclipse/plugins/com.st.tools.spc5.tools.gnu.gcc.ppcvle.win32_4.9.4.202511271245/toolchai...

Pooja1 by Associate II
  • 211 Views
  • 1 replies
  • 0 kudos

Resolved! Which MCAN should i select for CAN7 sys1

i'm using SPC58EC80E5 in that pin number 28 TX and 29 RX , in low level drivers configuration i dont know which MCAN to be select please help me and also if i want to configure any other CAN ,which MCAN i should select. below is my configuration scre...

Pooja1 by Associate II
  • 263 Views
  • 1 replies
  • 0 kudos

Resolved! AEK_POW_BMSNOTX (L9963E) cell voltage measurement

Evaluating the L9963E BCC chip for a BMS design, using the AEK_POW_BMSNOTX eval board together with AEK-MCU-C4MLIT1 (spc58ec) running the example BMS application as reference but seeing some odd results in the cell voltage readings.All readings are a...

Resolved! Issue with some errors(Undefined errors)

Hi all,While implementation of CanTp, I am getting some errors regarding undefined reference which are shown in the snippet attached. I debugged completely but I am unable to find from where and for what these errors are coming.It would be more helpf...

shiva_shankar_e_0-1725353272999.png