cancel
Showing results for 
Search instead for 
Did you mean: 

AEK-POW-BMS63EN as a Master Board in the daisy chain

MaraLo
Associate II

Hi,

I would like to check if STM AEK-POW-BMS63EN board can be used as a first board in the daisy chain with the setup where we have external MCU (for example STMF103RB) and AEK-COM-ISOSPI1?

In the datasheet you describe difference between 'Master' and 'Slave' in the following way:

MaraLo_0-1708798358615.png

and all your AEK-POW-BMS63EN comes with SPEIN pin pull-down via R20:

 

MaraLo_2-1708798811017.png

Can you please clarify if the usage of AEK-POW-BMS63EN in the single BMS setup with external MCU is even possible?

BR,

MaraLo

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Max VIZZINI
ST Employee

hi,

Yes, for a single node you can use STM32 SPI to AEK-COM-ISOSPI1 and connect the AEK-COM-ISOSPI1 to the AEK-POW-BMS63EN.

Be careful that endianess of STM32 and SPC5 is different (big endian).

Best Regards,

AutoDevKit Team

 

View solution in original post

1 REPLY 1
Max VIZZINI
ST Employee

hi,

Yes, for a single node you can use STM32 SPI to AEK-COM-ISOSPI1 and connect the AEK-COM-ISOSPI1 to the AEK-POW-BMS63EN.

Be careful that endianess of STM32 and SPC5 is different (big endian).

Best Regards,

AutoDevKit Team