BMS63EN Example does not start
- December 10, 2023
- 4 replies
- 4396 views
I imported the SPC58EC - AEK_POW_BMS63EN_SOC_Estimation_Single application, configured like described in UM3185.
(Side note: The Board View may also view that the ISO SPI needs a Powersupply... So I wonder the Generic pins table..shall I do something here or is it just info?)
When I connect the BMS63EN to the battery pack, the green LED flashes very shortly, than no further signs of live.
When I flash the AEK-MCU_C44MLIT1 nor errors are shown, though only one core is used, I think thats ok?
When I restart the MCU the debugger shows its running, LED 1 and 3 are green.
When connecting the ISO SPI to the BMS63EN nothing happens while MCU is without power.
Turning on Power to the MCU:
On the ISO SPI the red, blue and green LED are lit.
Nothing on the BMS63EN is lit.
->Closed the debugger (UDE), restarted for safety everything, opened Autodevkit, Window->Show View->other->terminal->terminal.
I opened Terminal on both available COM Ports, on both speeds 115200 and the older mentioned 38400 and receive: NOTHING.
Shouldn't the example application somehow communicate? Do I need to start it somehow? How?