cancel
Showing results for 
Search instead for 
Did you mean: 

[CubeIDE BUG] NVIC_ISER1-NVIC_ISER4 have wrong addresses at SFR view for NUCLEO F411RE

angelosn
Associate

Using the Cortex-M4 Devices Generic User Guide at page 219 it is written the address of ISERs

0xE000E100- 0xE000E11C NVIC_ISER0- NVIC_ISER7

While I was trying to debug my program I realized that these addresses in the IDE are wrong as you can see in the picture

0693W000007BjXeQAK.pngI hope that bug could be confirmed and fixed

If there is another place that I can post it please direct me to that.

STM32CubeIDE Version: 1.5.1 Build: 9029_20201210_1234 (UTC) Windows 10

1 ACCEPTED SOLUTION

Accepted Solutions
mattias norlander
ST Employee

This issue should be fixed in CubeIDE 1.7.0.

ST Internal ticket reference 109845.

View solution in original post

2 REPLIES 2
xtm
Associate

I have the same problem with Version: 1.6.1, Build: 9958_20210326_1446 (UTC)

mattias norlander
ST Employee

This issue should be fixed in CubeIDE 1.7.0.

ST Internal ticket reference 109845.