cancel
Showing results for 
Search instead for 
Did you mean: 

How to find the CubeIDE on my Mac?

burghard
Associate

After I installed the CubeIDE (STM32CubeIDE-Mac) on my mac with the delivered iinstaller, I cannot find the CubeIDE what is the name of the application? in which folder it is installed?

1 ACCEPTED SOLUTION

Accepted Solutions
burghard
Associate

The Solution to this was the the PKG Archive consists of two things - an installer for a server application which I executed and an application file wich has to be copied into te application folder. 
this file was hides by the lower border of the window in which the contents of the PKG file. So I missed to copy it. After I did I have been able to find the IDE on my computer (-:

May be that the settings for the size of the icons in the finder on my computer ist the reason for my mistake. 

 

View solution in original post

3 REPLIES 3
Andrew Neil
Super User

On windows, you can just search for it - does Mac not have that??

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
emrys57
Associate

It should be in /Applications/STM32CubeIDE.app

It may ask you to download the st-link server, when you run the debugger. Download that from
https://www.st.com/en/development-tools/st-link-server.html
and unzip it and run the mac installer .pkg file in there. On my machine, that installs /usr/bin/local/stlink-server

However, since updating to macOS 15.0 Sequoia, the IDE can no longer find the st-link-server.
https://community.st.com/t5/stm32-mcus-boards-and-hardware/st-link-server-is-required-error-after-macos-update/m-p/719798#M21344
https://stackoverflow.com/questions/78996974/stm32cubeide-debugger-no-longer-works-in-macos-15-0-sequoia

I still don't have mine working. Good Luck!

burghard
Associate

The Solution to this was the the PKG Archive consists of two things - an installer for a server application which I executed and an application file wich has to be copied into te application folder. 
this file was hides by the lower border of the window in which the contents of the PKG file. So I missed to copy it. After I did I have been able to find the IDE on my computer (-:

May be that the settings for the size of the icons in the finder on my computer ist the reason for my mistake.