cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIDE and STM32CubeMx bugs on Mac Catalina

AVoel.1
Associate III

These two bugs seem related.

Bug 1 on STM32CubeIDE. After modifying an ioc file, when you regenerate, the IDE wipes all the contents of the Drivers folder and all subfolders, and doesn't replace them! Yow.

Bug2 on STM32CubeMx. When generating code, the Core files are successfully created, but then STM32CubeMx hangs indefintely trying to create libraries.

Probably some problem with write permissions on Mac Catalina...

2 REPLIES 2
Khouloud ZEMMELI
ST Employee

Hi @AVoel.1​ ,

Are you still facing same issues with the latest CubeMX version (6.1.0) ?

Khouloud

AVoel.1
Associate III

No, actually. The problem went away by itself. I'm not sure if it was because of an update or not, but in any case, all is well. I'm grateful that ST is supporting the Mac OS platform. I abandoned Windows during the Windows 8 debacle and every time I have to do something in Windows I have to hold my nose. I was actually happy with Windows 7, I don't know why MS took such a wrong turn.