Skip to main content
urbito
Senior II
March 8, 2024
Solved

Texts Table and Text Area Widgets

  • March 8, 2024
  • 1 reply
  • 1060 views

Hello Community,

 

I have been working in an app that has 2 different lenguages defined in the "Texts" option in TouchGFX.

 

In the Canvans i have for example a textArea that is configured as "Auto-size" with typography "Large, 40px" and centered alignment, this text is in english "Select a Cycle" and in spanish is "Seleccione un Ciclo".

 

As there is the option to "Auto-size" the textbox, is there an option or a way to use instead an auto typography to adjust to the textbox? saying that both my text fit in the same TextBox, one with "Large, 40px" and the other with "Default, 25px".

 

Hope to hear from you soon :)

 

Greetings!

This topic has been closed for replies.
Best answer by urbito

The solution is in this post:

Using separate typographies for separate languages... - STMicroelectronics Community

 

The typography that the TextBox uses, can be configured for each lenguage to have different size/etc.

 

Greetings.

1 reply

urbito
urbitoAuthorBest answer
Senior II
March 8, 2024

The solution is in this post:

Using separate typographies for separate languages... - STMicroelectronics Community

 

The typography that the TextBox uses, can be configured for each lenguage to have different size/etc.

 

Greetings.