2024-03-08 02:44 AM - edited 2024-03-08 02:44 AM
Hello Community,
I have been working in an app that has 2 different lenguages defined in the "Texts" option in TouchGFX.
In the Canvans i have for example a textArea that is configured as "Auto-size" with typography "Large, 40px" and centered alignment, this text is in english "Select a Cycle" and in spanish is "Seleccione un Ciclo".
As there is the option to "Auto-size" the textbox, is there an option or a way to use instead an auto typography to adjust to the textbox? saying that both my text fit in the same TextBox, one with "Large, 40px" and the other with "Default, 25px".
Hope to hear from you soon
Greetings!
Solved! Go to Solution.
2024-03-08 03:14 AM
The solution is in this post:
Using separate typographies for separate languages... - STMicroelectronics Community
The typography that the TextBox uses, can be configured for each lenguage to have different size/etc.
Greetings.
2024-03-08 03:14 AM
The solution is in this post:
Using separate typographies for separate languages... - STMicroelectronics Community
The typography that the TextBox uses, can be configured for each lenguage to have different size/etc.
Greetings.