User Activity

STM32U0 is the first Cortex-M0+ with a static consumption of only 160 nA in standby mode with RTC (Real-Time Clock) and 16 nA in shutdown. It also achieves 118 points in CoreMark and targets SESIP level 3 and PSA level 1 focusing on firmware code pro...
The new STM32H7R/S lines are built on the success of the STM32H7 series, offering even higher performance and security at a lower cost. The STM32H7R/S is a bootflash-based MCU powered by a Cortex®-M7 core running up to 600 MHz, with 64 KB of user fla...
NanoEdge AI Studio v4.3 is now offered for free to all engineers, giving them the opportunity to create highly efficient TinyML libraries that can be deployed on Cortex-M based microcontrollers. In addition, other enhancements have been integrated to...
The STM32H573I-DK is now available for order! It is the first kit to support Secure Manager, a turnkey system-on-chip that integrates core security services certified and maintained by ST. The STM32H573I-DK enables developers to explore all the integ...
We are pleased to announce that the latest version of NanoEdge AI Studio is now available. This new version brings improvements in performance and support for STM32 boards, as well as new features to help users earlier in the creation of their machin...