2025-02-12 12:35 PM
im having trouble displaying my own bitmap what converter should i use to convert a bmp file to array to work with this function
2025-02-20 5:35 AM
Hi @Franksterb92 ,
Some converters may be used to convert the input image to a C or a header file.
In AN4861, "LCD image converter tool" is used to generate required input file.
You can refer to the paragraph "Display an image from the internal flash" for more details.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.