2023-12-07 1:42 AM - edited 2023-12-07 1:42 AM
NanoEdge AI Studio v4.3 is now offered for free to all engineers, giving them the opportunity to create highly efficient TinyML libraries that can be deployed on Cortex-M based microcontrollers. In addition, other enhancements have been integrated to support users in project creation and model selection.
You can download it here.
What is new in NanoEdge AI Studio V4.3?
Feel free to learn more about NanoEdge AI Studio by looking into our documentation!
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-01-09 11:43 AM
Hello, I have installed the application and I have no license key, can you please assist?
Thanks
2024-01-10 12:21 AM
Hello,
Normally, when downloading the installer, you have received an email with your license key. Please look for an email sent by noreply@nanoedgeaistudio.net
Else you can create a new license by filling this form: Download NanoEdge AI Studio - STMicroelectronics - STM32 AI
(you will receive a new email with your license)
Best regards,
Julian
2024-01-16 11:33 AM
@Amel NASRI : do you have any example that work in Anomaly Detection using the X-NUCLEO-IKS01A3 and NUCLEO-H743ZI2?
Thank you in advanced
2024-01-17 12:32 AM
Hello Alessandro,
I don't have specific example for the boards you mentioned, but you can take a look at this git repository.
It contains C code examples with the datalogging part and the use of NanoEdge AI Libraries.
Make sure to clone the repository using this command (with the submodules):
git clone https://github.com/stm32-hotspot/stm32ai-nanoedge-datalogger --recurse-submodules
Best regards,
Julian
2024-01-17 3:56 AM
Ok @Julian E. .
Thank you for this.
I will try start based on the github content.
Regards.