User Activity

Hi, I ran into a weird issue initializing a VL53L8CX over SPI where the firmware was seemingly failing to load correctly (the firmware checksum was wrong, and trying to read back some of the firmware from the sensor showed that it didn't match the da...
I'm looking into using the VL53L7CX on a board designed for the VL53L5CX. I expected it to be a drop-in replacement on the hardware side with only a change in software needed (using the L7CX API instead of the L5CX API), but when I compared the two A...
I'm testing the VL53L5CX and finding that the behavior of the LPn pin differs from what is described in the datasheet. The datasheet says "Drive this pin to logic 0 to disable the I2C comms when the device is in LP mode. Drive this pin to logic 1 to ...
I haven't been able to find a recommended footprint (PCB pad layout) for the VL53L5CX, either in the datasheet or anywhere else. When will that be available? Or did I miss it somewhere?
Kudos from
Kudos given to